Skip to main content
MBASL.1
Associate
June 24, 2020
Question

Unexpected restart, NUCLEO-L432KC

Hello,

I want to use a NUCLEO-L432KC as an interface card on a computer.

The L432KC reboots when it is plugged into the USB port of my computer in Windows 10.

These restarts occur randomly after a few minutes.

These restarts also occur if I supply it with 12V and it is connected to the USB port of the computer.

I did not observe these restarts when the L432KC is powered without being plugged into a USB port.

I did not observe these reboots when plugged into the USB port of another computer in Windows 7 and in Linux computer (Ubuntu 18.04).

Here is my test code:

#include "mbed.h"
 
 
 
DigitalOut myled (LED1);
 
DigitalIn button (PA_7);
 
 
 
int main () {
 
 while (! button) {
 
 myled = 1; // LED is ON
 
 wait (1.0); // 1 seconde
 
 myled = 0; // LED is OFF
 
 wait (1.0); 
 
 }
 
 while (1) {
 
 myled = 1; // LED is ON
 
 wait (0.25); // 250 ms
 
 myled = 0; // LED is OFF
 
 wait (0.25); 
 
 }
 
}

A button is connected between PA_7 and + 5V, a restoring resistor (15kohm) between PA_7 and GND.

At startup (or restart) the LED flashes at 0.5 Hertz, after pressing the button connected to PA_7 the LED flashes at 2Hz.

If you have an idea on the origin of the problem ?

Marc.

This topic has been closed for replies.

1 reply

MBASL.1
MBASL.1Author
Associate
June 29, 2020

Hello,

I answer my own post:

I first tried to update the ST-LINK driver

After that, I had to restart the computer, the operation was not yet stable (I had the impression that things were continuing to implement this in Windows 10).

I then installed the ST-LINK firmware update

After that, I restarted the computer again, the operation was still not stable (and I still had the impression that things continued to set it up).

I installed ST-LINK utility

Then I restart. It functioned. But I don't think the ST-LINK utility had anything to do with it. I thought rather that it was the update of the driver ST-LINK or the update of the firmware.

Marc.