Unexpected IDLE Interrupt with Full Buffer Size Before Any UART Data Received on STM32L433 (HAL_UARTEx_ReceiveToIdle_DMA)
- 1 reply
- 1617 views
Hello ST Community,
I’d like to report an issue observed with HAL_UARTEx_ReceiveToIdle_DMA() on STM32L433RCT6P using STM32CubeIDE v1.17.0 and the latest STM32CubeMX code generator (L4 series).
Setup:
Board: NUCLEO-L433RC-P
IDE: STM32CubeIDE 1.17.0
HAL version: STM32CubeL4 latest
UART: USART2
DMA Mode: Circular
Baudrate: 115200
Buffer size: 128 or 256
Code: Generated with CubeMX
What we do:
Call MX_USART2_UART_Init()
Immediately call HAL_UARTEx_ReceiveToIdle_DMA() without delay
Do not send any UART data to the board
Wait...
What we expect:
The callback HAL_UARTEx_RxEventCallback() should not trigger until at least one byte has been received, followed by line idle.
What actually happens:
Immediately after startup, without any incoming UART data:
The callback fires once
Size == RX_BUFFER_SIZE (e.g., 128 or 256)
Additional Observations:
The issue doesn't occur at very low system clock frequencies
On STM32L4 series: it triggers when running on HSI (16 MHz)
When using MSI @ 4 MHz, the issue does not occur
On STM32U5 series (e.g., STM32U595), the threshold frequency differs but the pattern is the same
Why this matters:
As part of building high-quality embedded platforms, we aim to avoid:
Arbitrary HAL_Delay() or for(__NOP()) hacks
Fragile time-based fixes that behave differently across platforms or temperature/voltage conditions
We need a deterministic solution to prevent this false RX interrupt on startup.
Reproduction Snippet: (A simple example code snippet)
#define RX_BUFFER_SIZE 128
uint8_t aRXBufferUser[RX_BUFFER_SIZE];
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
HAL_UARTEx_ReceiveToIdle_DMA(&huart2, aRXBufferUser, RX_BUFFER_SIZE);
while (1) {}
}
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
//echo back the received size
uint8_t low = Size & 0xFF;
while (!(__HAL_UART_GET_FLAG(huart, UART_FLAG_TXE))) {}
huart->Instance->TDR = low;
}
My Questions to ST:
Why does HAL_UARTEx_RxEventCallback() trigger immediately with Size == buffer_size, even though no data was received?
- Is there a documented correct sequence or flag to wait for before calling HAL_UARTEx_ReceiveToIdle_DMA()?
- What is the correct way to prevent this spurious interrupt from happening without using arbitrary HAL_Delay()?
Attached Video Evidence:
I’ve attached a short video demonstrating the issue:
When using MSI @ 4 MHz, no interrupt is triggered → expected behavior
When switching to HSI @ 16 MHz, the interrupt fires immediately after HAL_UARTEx_ReceiveToIdle_DMA()→ even though no data is received
The video shows a breakpoint inside HAL_UARTEx_RxEventCallback() and proves the size equals the buffer length, with no bytes transferred by DMA.