Skip to main content
MSher.1
Associate II
Sep 24, 2021 3:22 PM UTC
Solved

Unable to wake task from event flag in ISR when USB_FS is enabled using CMSIS OS 2 on STM32L5

I have been using USB_FS for some time now and recently added the EXT13 IRQ for the user button in the STM32L5 DK. I set a task to toggle a pin when the button is pressed and noticed that if the USB is running, the event does not wake the user button task. If the USB is disabled or does not start properly, the task wakes and functions as expected. If I remove the event flag wait, the task functions normally. I have tried both IRQ priorities equal and lowering the USB priority with the same result that the task does not wake when the USB is active.

This topic has been closed for replies.
MSher.1
MSher.1Best answer
Associate II
Oct 6, 2021 5:57 PM UTC
Hi Walid,
Thanks for the reply. Unfortunately, I’ve already moved on with a different approach using osThreadFlagsSet/Wait and don’t have the time to recreate the previous iteration. In the future, I will save the code in the troubled state for reference.
Best regards,
Michael

3 replies

Walid ZRELLI
Visitor II
Oct 6, 2021 3:58 PM UTC

Hello @MSher.1​ ,

Can you please provide your project for further check?

Thanks in advance.

BeST Regards,

Walid

MSher.1
MSher.1AuthorBest answer
Associate II
Oct 6, 2021 5:57 PM UTC
Hi Walid,
Thanks for the reply. Unfortunately, I’ve already moved on with a different approach using osThreadFlagsSet/Wait and don’t have the time to recreate the previous iteration. In the future, I will save the code in the troubled state for reference.
Best regards,
Michael
Walid ZRELLI
Visitor II
Oct 7, 2021 8:07 AM UTC

Hello @MSher.1​ ,

Thanks for your feedback :smiling_face_with_smiling_eyes:

BeST Regards,

Walid