Skip to main content
Associate II
October 16, 2023
Question

unable to read port memory

  KeyInputMemory[column_count] = (uint16_t)(GPIOB->IDR);

       uint16_t mask = 0x0FFF;

       KeyInputMemory[column_count] &= mask;

 

    if (KeyInputMemory[column_count] == StoredKeyInput[column_count]) {  //

 

        KeyInputCounter[column_count]++;

        if (KeyInputCounter[column_count] > 5) {

        

            StoredKeyInput[column_count] = KeyInputMemory[column_count];

 

            // Reset the counter

          //KeyInputCounter[column_count] = 0;

        }

 

    } else {

        // Store the current key input into the column stored key input

        StoredKeyInput[column_count] = KeyInputMemory[column_count];

 

        // Clear the key input count

        KeyInputCounter[column_count] = 0;

 

        //EXIT

        return;

    } I have physical keyboard i have to read b port but not detecting is my logic is true or false....... whenever key is pressed not reading the values

This topic has been closed for replies.

2 replies

ST Technical Moderator
October 16, 2023

Hello @Girish1 

 

Would you provide more details about the issue? If possible, add more context about your Hardware setup, attach your IOC file/configuration.

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
TDK
October 16, 2023

The code doesn't make a whole lot of sense here. You're comparing 12 different bits in the code. I suspect you want to look at a single bit instead.

Suggest using HAL_GPIO_ReadPin instead if you're not comfortable with bitwise manipulation.

"If you feel a post has answered your question, please click ""Accept as Solution""."