Skip to main content
ShivaRagu
Senior
May 22, 2021 12:39 PM UTC
Question

UNABLE TO CONVERT TFLITE MODEL FROM KERAS MODEL

Hi,

Am trying to create the ASC model which is existing in FP-AI-SENSING1 Pack. When I was converting from keras model to TFlite model am getting below error. Am using the same code which is in the pack, am not changing anything. Even the audio files am using the same.

Anyone can help?

ERROR-

AttributeError: type object 'TFLiteConverter' has no attribute 'from_keras_model'

Below is the code which am using to convert into TFlite model.

def representative_dataset_gen():

    for i in range(len(x_train_r)):

        yield [x_train_r[i].reshape((1, ) + x_train_r[i].shape)]

converter = tf.lite.TFLiteConverter.from_keras_model(out_dir + "Outputmodel.h5" )

converter.optimizations = [tf.lite.Optimize.DEFAULT]

converter.representative_dataset = representative_dataset_gen

converter.target_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8]

converter.inference_input_type = tf.int8

converter.inference_output_type = tf.int8

tflite_model = converter.convert()

with open(out_dir + 'model.tflite','wb') as f:

    f.write(tflite_model)

    print("TFlite model saved")

    

Regards,

shankari.

This topic has been closed for replies.