Skip to main content
Associate
Sep 24, 2024 2:51 PM UTC
Question

UART DMA with RTOS

Hi all,
I spent hours but I cannot make UART work in DMA circular mode with RTOS (CMSIS V2).
Can someone send me a simple example ?
I would like to receive characters from PC (various length commands: 8-10 chars) and process them in another task parallel. Then save the position and next time start processing the commands in the buffer from the previous position.

What I experienced is that ReceiveBuffer contains one only character. When I put a breakpoint at HAL_UART_Receive_DMA line and send the characters, in next iteration I see the whole string received.
I guess somehow I have to wait till the streaming is finished.

Finally a made it work. Hw issue is always the last thing what I'm suspecting...
I haven't noticed this in device manager:

Adam90_0-1727526459199.png

Replacing the USB-UART converter solved the issue and uC receiving the incoming stream with DMA.

 

This snippet seems working:

 

 

void StartDefaultTask(void *argument)

{

HAL_UARTEx_ReceiveToIdle_DMA(&huart5, (uint8_t*)ReceiveBuffer, 256);

for(;;)

{

if(ReceiveBuffer[shift]!='\0')

{

osMessageQueuePut(MessageBufferQueueHandle, &(ReceiveBuffer[shift]), 0, 0); //saving to queue

ReceiveBuffer[shift]='\0';

shift++;

}

osDelay(50);

}

}

 

 

 

 

 

This topic has been closed for replies.

5 replies

ST Technical Moderator
Sep 24, 2024 5:47 PM UTC

Hello @Adam90 and welcome to the Community :)

Please take a look at this GitHub link.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Adam90Author
Associate
Sep 28, 2024 12:17 PM UTC

Thanks for the feedback. I've already seen this repo. 
My problem with this:
- it is using LL functions
- and it is saving the incoming stream to QUEUE instead of DMA

Karl Yamashita
Super User
Sep 24, 2024 11:11 PM UTC

We have no idea what you're doing. Show your interrupt code

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Pavel A.
Sep 28, 2024 8:17 PM UTC

> I've already seen this repo

Great so this is basically how it should be done. The cyclic DMA receiver can be combined with another component by Mr. Majerle, the ring buffer. The buffer used for DMA receive coincides with the software ring buffer so no copying is needed. The DMA interrupt handlers or callbacks only synchronize the pointers and signal the reader task that new data arrived. Waking the task is fast and does not involve moving any data or queues. Sorry I don't have a ready code to share but that's the idea.

 

 

 

Karl Yamashita
Super User
Sep 29, 2024 12:28 AM UTC

Don't edit your original post showing the fix. Some of us have already seen your post and are following along. In most cases, we are no longer looking at the 1st post, but the latter. I had no idea you found a fix because i wasn't notified by email.

To make it easier to follow along and not to see strike through your post, just reply with the fix, then mark it as the Accept as Solution

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source