Skip to main content
This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
Dec 16, 2021 10:54 PM UTC

Suggest you pick one post, and edit it to have summary, question, and context

Edit is in a small [V] icon, upper right of pane.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
GreenGuy
GreenGuyAuthor
Senior III
Dec 16, 2021 11:13 PM UTC

Sorry. Thought I was searching for an answer. It has been a very frustrating long day. I did try to delete both posts but the delete options responds that I am not allowed to delete.

waclawek.jan
Super User
Dec 16, 2021 11:21 PM UTC

And did you find the answer? If not, perhaps you may want to elaborate on description of the problem?

JW

GreenGuy
GreenGuyAuthor
Senior III
Dec 16, 2021 11:40 PM UTC

No I have not so here is the detail. Again I apologize for any confusion.

I am trying to use the Azure RTOS and the thread processes are working fine. I want to add queue handling so added a test queue.

After the thread creations and the event flags group I added:

 /* Create the Queues */

 //Allocate queue memory

 if (tx_byte_allocate(byte_pool, (VOID **) &pointer, MCU_CMD_QUEUE_SIZE*sizeof(ULONG), TX_NO_WAIT) != TX_SUCCESS)

 {

ret = TX_POOL_ERROR;

 }

 if (tx_queue_create(&Queue_CMD, "Queue MCU Command", TX_1_ULONG, pointer, MCU_CMD_QUEUE_SIZE*sizeof(ULONG)) != TX_SUCCESS)

 {

  ret = TX_QUEUE_ERROR;

 }

Later in the code I try to send a message with:

ULONG message;

message =1;

status = tx_queue_send(&Queue_CMD, &message, TX_WAIT_FOREVER);

 if (status != TX_SUCCESS)

   {

    Error_Handler();

   }

The code ends up in the fault handler.

Can't figure out why.

Haithem Rahmani
ST Employee
Dec 19, 2021 11:20 AM UTC

Hi @Community member​ 

Could you please give more details about your test.

  • Which STM32 are you using?
  • Are you using any X-CUBE-AZRTOS package?
  • On which toolchain are you using?

regards

Haithem

GreenGuy
GreenGuyAuthor
Senior III
Dec 20, 2021 5:46 PM UTC

STm32H723ZG Nucleo board

AZRTOS - 2.0.0

STM32CubeIDE - GNU(9-2020-q2-update)

I did find in the STM32H723ZGTX_FLASH.ld that the ._threadx_heap assignment was missing. I thought that odd since this was taken from the Tx_Thread_Creation example application for the nucleo board I am using. That example was working before I added the use of a queue and perhaps no assignment in the linker is needed when not using message queues. At the moment I amusing:

._threadx_heap

{

. = Align(8);

_RAM_segment_used_end__ = .;

. = . + 32K;

. = ALIGN(8);

} >RAM_D1

The section above is placed after .bss and before ._user_heap_stack.

However I am still ending up in the HardFault_Handler.

The HFSR->FORCED is set and the CFSR->BFARVALID and CFSR->PRECISERR are set.

waclawek.jan
Super User
Dec 17, 2021 8:48 AM UTC

Which STM32?

This will be Azure-specific so you should perhaps seek help at their support, if there's any. Don't think he are any Azure users. Also you can try to debug as hardfaults are devices usually - look at the fault registers, and also from the stacked PC and disasm look up the offending instruction and if it's a portion to which you have the sources, you may estimate the reason.

JW