Skip to main content
SBaro.11
Associate III
Apr 17, 2024 2:48 PM UTC
Question

Trying to adapt stm32f4 for stm32l452RE

Hi all,

I'm truying to adapt one file coming fromm stm32f4 discovery board for using UART. But when I try to add it to my STM NUCLEO L452RE board I got an error :

 

 

 

 

../Drivers/BSP/uart.c:328:63: error: 'USART_TypeDef' has no member named 'DR'; did you mean 'RDR'?
 328 | data = (uint8_t) ((uint16_t) (s_uart1Handle.Instance->DR & (uint16_t) 0x01FF) & (uint16_t) 0x00FF);
 | ^~
 | RDR

 

 

 

  

Here is the function :

 

 

 

 

void USART1_IRQHandler(void)
{
 uint8_t data;
 uint16_t usedCapacityOfBuffer = 0;
 uint16_t realCountPutBuffer = 0;

 if (__HAL_UART_GET_IT_SOURCE(&s_uart1Handle, UART_IT_RXNE) != RESET &&
 __HAL_UART_GET_FLAG(&s_uart1Handle, UART_FLAG_RXNE) != RESET) {
 data = (uint8_t) ((uint16_t) (s_uart1Handle.Instance->DR & (uint16_t) 0x01FF) & (uint16_t) 0x00FF);
 realCountPutBuffer = RingBuf_Put(&s_uart1ReadRingBuffer, &data, 1);
 usedCapacityOfBuffer = UART1_READ_BUF_SIZE - RingBuf_GetUnusedSize(&s_uart1ReadRingBuffer);
 s_uart1ReadBufferState.maxUsedCapacityOfBuffer =
 usedCapacityOfBuffer > s_uart1ReadBufferState.maxUsedCapacityOfBuffer ? usedCapacityOfBuffer
 : s_uart1ReadBufferState.maxUsedCapacityOfBuffer;
 s_uart1ReadBufferState.countOfLostData += 1 - realCountPutBuffer;
 }

 if (__HAL_UART_GET_IT_SOURCE(&s_uart1Handle, UART_IT_TXE) != RESET &&
 __HAL_UART_GET_FLAG(&s_uart1Handle, UART_FLAG_TXE) != RESET) {
 if (RingBuf_Get(&s_uart1WriteRingBuffer, &data, 1)) {
 /* Transmit Data */
 s_uart1Handle.Instance->DR = ((uint16_t) data & (uint16_t) 0x01FF);
 } else {
 __HAL_UART_DISABLE_IT(&s_uart1Handle, UART_IT_TXE);
 }
 }
}

 

 

 

 

Do you think I can change DR by RDR? What is the difference, I've lookin for but I don't find good explaination...

Should I used TDR for transmit and RDR for receive maybe ?

Thanks

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
Apr 17, 2024 2:53 PM UTC

@SBaro.11 wrote:

Do you think I can change DR by RDR? What is the difference,


Look at the two different definitions of the USART_TypeDef structure for the two different processors (L4 and F4).

Also look at the register definitions (in the Reference Manuals) for the two processors (L4 and F4).

That should tell you if they're compatible ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.