Skip to main content
AElta.1
Associate II
Sep 21, 2022 7:07 AM UTC
Question

Transmit data through CDC VCP Failed error

I am trying transmit data using CDC(virtual port) in NUCLEO-H743Zi2, but I am getting this error when I plug in my VCP port to my pc (Unknown USB Device (Device Descriptor Request Failed)), I could not find a way to fix it.

My hardware settings:

MCU speed set to MAX(480Mhz)

USB_OTG_FS : Device Only | VBUS sensing | enabled Activate SOF

USB_Device : CDC(VPC).

my transmission code:

/* USER CODE BEGIN PD */
#include "main.h"
#include "usb_device.h"
#include "usbd_cdc_if.h"
#include "string.h"
/* USER CODE END PD */
char *data = "Hello there";
int main(void)
{
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 /* Configure the system clock */
 SystemClock_Config();
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART3_UART_Init();
 MX_DMA_Init();
 MX_SPI1_Init();
 MX_USB_DEVICE_Init();
 /* Infinite loop */
 while (1) {
 /* USER CODE END WHILE */
 	CDC_Transmit_FS((uint8_t *) data , strlen(data));
 	 	HAL_Delay (1000);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

The debugging steps I followed:

  1. Changed min heap size = 0x2000 and min stack size = 0x2000 (I tried several values)
  2. downloaded the VCP driver even though I am using win10.
  3. The global interrupt is enabled.
  4. set get Line coding function:
USBD_CDC_LineCodingTypeDef LineCoding = {
 115200, /* baud rate */
0x00, /* stop bits-1 */
 0x00, /* parity - none */
 0x08 /* nb. of bits 8 */
};
static int8_t CDC_Control_FS(uint8_t cmd, uint8_t* pbuf, uint16_t length)
{
switch(cmd)
 {
case CDC_SET_LINE_CODING:
 LineCoding.bitrate = (uint32_t) (pbuf[0] | (pbuf[1] << 8) |
 	 (pbuf[2] << 16) | (pbuf[3] << 24));
 	 LineCoding.format = pbuf[4];
 	 LineCoding.paritytype = pbuf[5];
 	 LineCoding.datatype = pbuf[6];
 break;
 
 case CDC_GET_LINE_CODING:
 	 pbuf[0] = (uint8_t) (LineCoding.bitrate);
 	 pbuf[1] = (uint8_t) (LineCoding.bitrate >> 8);
 	 pbuf[2] = (uint8_t) (LineCoding.bitrate >> 16);
 	 pbuf[3] = (uint8_t) (LineCoding.bitrate >> 24);
 	 pbuf[4] = LineCoding.format;
 	 pbuf[5] = LineCoding.paritytype;
 	 pbuf[6] = LineCoding.datatype;
break;
...
 }
 
 return (USBD_OK);
 /* USER CODE END 5 */
}

But still I am getting (Unknown USB Device (Device Descriptor Request Failed) before running the code and after.

This topic has been closed for replies.

5 replies

ST Technical Moderator
Sep 21, 2022 9:41 AM UTC

Hello @AElta.1​ 

Do you have drivers installed STM32 Virtual COM Port Driver ?

 I advise you to follow this FAQ: USB device not recognized, it may help you:

  • Try increase the heap size or configure the USB library to use static allocation, as recommended in the FAQ.

You may get inspired from CDC_Standalone examples within STM32H7 MCU package, which can help you to develop your application:

\STM32Cube_FW_H7_V1.10.0\Projects\STM32H743I-EVAL\Applications\USB_Device\CDC_Standalone\

Note: When DMA is used, the MX_DMA_Init shall always be called before any other  peripheral initialization. Please refer to this post.

Please keep me informed if you still need help.

If my answer fully solved your issue, please mark it as best by clicking on the "Select as Best" button. This will help other users find this solution more quickly.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
AElta.1
AElta.1Author
Associate II
Sep 22, 2022 7:39 AM UTC

hi I tried what u suggested but I am sill facing the same issue

0693W00000SvyAbQAJ.png

ST Technical Moderator
Sep 22, 2022 2:37 PM UTC

Check if USB_OTG_FS_DP and USB_OTG_FS_DM wires are swapped.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks