Skip to main content
STE_Michael
Associate
Dec 1, 2023 12:30 PM UTC
Question

Touch Sensing Library (STM32Cube_FW_L0_V1.12.1) uses delay which depends on fixed system clock!

In STM32Cube_FW_L0_V1.12.1\Middlewares\ST\STM32_TouchSensing_Library\src\tsl.c, the value TSL_Globals.DelayDischarge is initialized in TSL_Init() as:

TSL_Globals.DelayDischarge = (uint32_t)((TSLPRM_DELAY_DISCHARGE_ALL * (uint32_t)(SystemCoreClock /1000000)) / 72); 

It is noticeable that :
- 72 is used as magicNumber
- DelayDischarge also changes when the SystemClock is changed, i.e. when the main clock of the STM32 is changed, the behavior of the touch evaluation could change unexpectedly.

- What is with IAR Compiler?

TSL_Globals.DelayDischarge is only used for the SoftDelay() function tsl_acq_tsc.c

/**
 * @brief Software delay (private routine)
 * @param val Wait delay
 * @retval None
 * @note Measurements done with HCLK=72MHz and Keil/MDK-ARM compiler
 * val = 500: ~ 63us
 * val = 1000: ~126us
 * val = 2000: ~251us
 */
void SoftDelay(uint32_t val)
{
 volatile uint32_t idx;
 for (idx = val; idx > 0; idx--)
 {}
}

This is therefore only a software delay. The commentary shows that the approximate values were measured with a main clock of HCLK=72MHz. This is presumably where the magicNumber 72 above comes from. So if the value of DelayDischarge should not depend on the SystemClock, the assignment in TSL_Init() would probably have to be changed.

The question is whether other delay functions are available for SoftDelay(), which delay a microsecond duration independently of the system clock so that the touch parameters (especially TSLPRM_DELAY_DISCHARGE_ALL) do not depend on the system clock.

This topic has been closed for replies.

1 reply

Stassen.C
ST Employee
Dec 1, 2023 1:36 PM UTC

Hi STE_Michael,

You are right it is only a software delay and this allows that all capacitors to be completely discharge.
The formula

TSL_Globals.DelayDischarge = (uint32_t)((TSLPRM_DELAY_DISCHARGE_ALL * (uint32_t)(SystemCoreClock /1000000)) / 72); 

is linked to the system clock, there is a define in the tsl_conf.h

#define TSLPRM_DELAY_DISCHARGE_ALL (1000)

You can update this value to get your desired delay. For now we don't have any other function doing this.

I hope I answered your question

 


Regards
Stassen

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.