Skip to main content
BSarn.1
Associate
Nov 22, 2022 8:32 AM UTC
Question

Timer IT stop channel, but continue with base IT possible?

Calling HAL_TIM_OC_Stop_IT causes HAL_TIM_Base_Start_IT to also stop, is this normal? i want to stop a channel, not the entire base timer.

How do i achieve this? re-enabling the base timer after stopping the Channel is not working.

This topic has been closed for replies.

5 replies

Piranha
Principal III
Nov 22, 2022 11:14 PM UTC

It's all the same for HAL_TIM_OC_Stop(), HAL_TIM_OC_Stop_IT(), HAL_TIM_OC_Stop_DMA() functions.

https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_tim.c#L858-L865

Edited by moderation team to adhere to community guidlines.

Piranha
Principal III
Dec 3, 2022 4:33 PM UTC

Actually it's even worse - just search for all instances of "__HAL_TIM_MOE_DISABLE" in that file and all of those functions are broken the same way. Therefore the affected functions can be described as:

HAL_TIM_***_Stop***()

Amel NASRI
ST Technical Moderator
Dec 2, 2022 9:56 AM UTC

Hi @BSarn.1​ ,

I reported this issue to our development team for deeper analysis. Meanwhile, could you please try to use the LL drivers?

Internal ticket number: 140440(This is an internal tracking number and is not accessible or usable by customers).

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
BSarn.1
BSarn.1Author
Associate
Dec 2, 2022 10:22 AM UTC

i have solved for myself but i had to make a modification into the stm32f4xx_hal_tim.c

on line 1011 i have made:

 /* Disable the Peripheral */
 //__HAL_TIM_DISABLE(htim); //removed manually

then the base timer will continue as i desire.

S.Ma
Principal
Dec 5, 2022 2:55 AM UTC

A dirty workaround would be to disconnect the timer signal from ita pin by changin MODE bitfield from 10b