Skip to main content
Senior
Jan 29, 2026 6:51 PM UTC
Solved

Timer and ADC on STM32F429

Hi,

I want to kick ADC1 IN5 with the Timer TIM2. 

I'm working with CubeIDE.

I select:

ADC1 -> ADC_Regular_Conversion_Mode -> External Trigger Conversion Source  -> Timer 2 Trigger Out event

TIM2 ->  Trigger Output (TRGO) Parameters -> Update Event

But ADC1 does not run, Data Register is constant.

If I kick ADC1 by software everything is fine, I get some noisy numbers.

TIM2 is running, the count register is counting.

Why does TIM2 not kick ADC1 by the TRGO event?

This setup used to work fine on STM32F303. 

What do I miss on the STM32F429?

THX Cheers

Detlef 

Karl Yamashita
Karl YamashitaBest answer
Principal
Jan 31, 2026 1:44 AM UTC

I took your IOC file and generated a project. I'm not sure if there is a reason you're using PWM with no output for Timer1 but I don't see an Option for the ADC to use an appropriate trigger from Timer1.  I used Timer 3 which the ADC can trigger off the Trigger Out Event. I attached the updated IOC file.

 

I always use DMA so i use HAL_ADC_Start_DMA. But I noticed that you're using  HAL_ADC_Start in which the DR register value does not update. But if I use HAL_ADC_Start_IT, the DR register value updates. 

Either HAL_TIM_Base_Start_IT or HAL_TIM_Base_Start works. But with your Counter Period at 71 (1.69us), it is too fast so the Timer Interrupt keeps the main while loop from running. If you plan to send this ADC value as telemetry data, then HAL_TIM_Base_Start will work best.

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source

18 replies

Karl Yamashita
Principal
Jan 29, 2026 11:14 PM UTC

You haven't mentioned that you've called HAL_TIM_Base_Start_IT

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
DetlefSAuthor
Senior
Jan 29, 2026 11:56 PM UTC

I started both TIM and ADC. I printed out the timer count values, they change. So the counter is up and running. I kicked the ADC with software and got noisy numbers in the data register. So the ADC is up as well. Update should result in trigger out event for the timer. Trigger out event for the timer should fire up ADC. That does not happen.

 

It works for STM32F303.

What do I miss for STM32F429 ?

THX

Cheers

Detlef

Karl Yamashita
Principal
Jan 30, 2026 12:07 AM UTC

@DetlefS wrote:

I started both TIM and ADC.


This could mean anything. Show your code. 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
waclawek.jan
Super User
Jan 30, 2026 10:21 AM UTC

Read out and check/post content of TIM and ADC registers.

JW

Karl Yamashita
Karl YamashitaBest answer
Principal
Jan 31, 2026 1:44 AM UTC

I took your IOC file and generated a project. I'm not sure if there is a reason you're using PWM with no output for Timer1 but I don't see an Option for the ADC to use an appropriate trigger from Timer1.  I used Timer 3 which the ADC can trigger off the Trigger Out Event. I attached the updated IOC file.

 

I always use DMA so i use HAL_ADC_Start_DMA. But I noticed that you're using  HAL_ADC_Start in which the DR register value does not update. But if I use HAL_ADC_Start_IT, the DR register value updates. 

Either HAL_TIM_Base_Start_IT or HAL_TIM_Base_Start works. But with your Counter Period at 71 (1.69us), it is too fast so the Timer Interrupt keeps the main while loop from running. If you plan to send this ADC value as telemetry data, then HAL_TIM_Base_Start will work best.

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
DetlefSAuthor
Senior
Feb 1, 2026 10:16 PM UTC

Hi,

sorry for the somewhat delayed answer, I crashed my development environment and had to set it up anew. The problem is solved . The ADC needs interrupt capabilities, both in the .ioc file and with HAL_ADC_Start_IT . This is not necessary for the Timer. It worked for STM32F303 because there I started from the beginning with DMA. This will be next, stay tuned ;) .

THX Cheers

Detlef

DetlefSAuthor
Senior
Feb 2, 2026 7:51 PM UTC

Hi,

DMA does not work :( . I added DMA 2 Stream 0 to ADC1. DMA 2 Stream 0 is configured as a circular buffer. In NVIC settings of ADC1 global interrupts  ADC1, ADC2 and ADC3  are enabled. DMA 2 Stream 0 is greyed out, I can not enable it.

I replaced

HAL_ADC_Start_IT(&hadc1);

with

HAL_ADC_Start_DMA (&hadc1, (uint8_t *) hugbuf, (uint16_t)HUGBUFLEN); 

I added 

HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef * hadc1)

HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef * hadc1)

 

but HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef * hadc1) is only called once.

 

What am I missing?

THX Cheers

Detlef

 

 

 

TDK
Feb 2, 2026 7:58 PM UTC

The code you shared doesn't use DMA at all.

The function HAL_ADC_Start_DMA works as intended. You can see an example of it being used here:

STM32CubeF4/Projects/STM324xG_EVAL/Examples/ADC/ADC_RegularConversion_DMA/Src/main.c at 7c6a0a09ecb81b360de396479e048907563f1d10 · STMicroelectronics/STM32CubeF4

 

> What am I missing?

Should we just guess or do you want to share relevant code? My crystal ball suggests DMA isn't configured in circular mode.

"If you feel a post has answered your question, please click ""Accept as Solution""."