Skip to main content
CSand
Senior
August 20, 2020
Question

TIM2 with RTOS PeriodElapsCallback executed once only

Hello,

I have a simple project. I'm using FreeRTOS and programmed TIM2 1ms interrupt.

The TIM2_IRQHandler and PeriodElapsCallback are only called once in the beginning but not after.

I set Clock at 64MHz, the PSC is 63999 and Counter period is 9 I expect 1ms interrupt. I set NVIC TIM2 global intterupt.

I intend to use vTaskNotifyGiveFromISR but first need to make TIM2 interrupt to work.

The real time tasks seem to work fine.

Currently I programmed a counter increment in the PeriodElapsCallback  to make sure it works.

I attached the project if someone can support and check. I am probably missing something.

Thanks

This topic has been closed for replies.

3 replies

CSand
CSandAuthor
Senior
August 20, 2020

I'm not sure what I've changed, in any case the PeriodElapseCallback works ok if I have the test increment counter code.

But I'm back in problems if I call vTaskNotifyGiveFromISR. I may not use correct task handler.

In the main.c file I have

extern osThreadId UserTaskIMUHandle;

and the call for vTaskNotifyGiveFromISR is

	 void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 /* USER CODE BEGIN Callback 0 */
 
 /* USER CODE END Callback 0 */
 if (htim->Instance == TIM1) {
 HAL_IncTick();
 }
 /* USER CODE BEGIN Callback 1 */
 if (htim->Instance == TIM2)
 {
	 BaseType_t xHigherPriorityTaskWoken;
	 xHigherPriorityTaskWoken = pdFALSE;
 
 
	 vTaskNotifyGiveFromISR( UserTaskIMUHandle, &xHigherPriorityTaskWoken );
	 portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
 }

In the freertos.c I have

void StartUserTaskIMU(void const * argument)
 {
  /* USER CODE BEGIN StartUserTaskSND */
 	uint32_t ulNotifyValue;
  
 for(;;)
  {
 	 ulNotifyValue = ulTaskNotifyTake(pdTRUE, 0xFFFFFFFF);
 	 if(ulNotifyValue != 0)
 	 {
 		 // User code
 	 }
 
 }

Would someone support to check if this is correct please?

Thanks

CSand
CSandAuthor
Senior
August 20, 2020

Some more details that I found ...

The run stops and holds in the Tasks.c file at line "configASSERT( xTaskToNotify )" in the function ...

void vTaskNotifyGiveFromISR( TaskHandle_t xTaskToNotify, BaseType_t *pxHigherPriorityTaskWoken )

 Should I suspect it is something about the task handler?

hs2
Visitor II
August 20, 2020

Double check that the tasks are created (and the assigned handle is not NULL) before arming the interrupt.