Skip to main content
Tobe
Senior III
Apr 19, 2023 9:33 AM UTC
Question

TIM1 input cpature with DMA: DMA happens at high level when there is no rising edge. [F303K8T6]

Hi,

i got some issue, where i restart a "5 times DMA" after i read the array. The first DMA is happening right after i startet it, when the level is high. But that is not a rising edge! I already made some test to verify this problem. The solution so far is, to wait for the signal to become low. But cpu time i valuable... A solution to this "solution" would be to check periodically is the signal is low, but that is also not so ideal (ugly and takes cpu time too).

in main loop:
 
if(dmaCompleted){
 
		dmaCompleted = false;
 
//		while(GPIOA->IDR & GPIO_PIN_8){
//			//print("wait\n", 5); //wait for pin to become low, as a high level (not rising edge) will falsly trigger a dma request!
//		}
		LED3_GPIO_PORT->BRR = (uint32_t)LED3_PIN;
 
		HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_1, tim1_cpat_1, 5);
 
	}
 
	
	
static void MX_TIM1_Init(void)
{
 
 /* USER CODE BEGIN TIM1_Init 0 */
 
 /* USER CODE END TIM1_Init 0 */
 
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_IC_InitTypeDef sConfigIC = {0};
 
 /* USER CODE BEGIN TIM1_Init 1 */
 
 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 65535;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_IC_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
 sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
 sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
 sConfigIC.ICFilter = 0;
 if (HAL_TIM_IC_ConfigChannel(&htim1, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM1_Init 2 */
 
 /* USER CODE END TIM1_Init 2 */
 
}
 
Interrupt:
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){
	LED3_GPIO_PORT->BSRR = (uint32_t)LED3_PIN;
	dmaCompleted = true;
}

Anyone has a solution, or can point me in the direction i can further investigate?

Cheers,

Toby

This topic has been closed for replies.