Skip to main content
NafiurRahman
Associate III
Jul 14, 2022 6:54 PM UTC
Question

Tickless Idle Mode not satisfying if( xModifiableIdleTime > 0 ).

Hi, I'm trying to use FreeRTOS Tickless idle mode. When I am debugging my code (using breakpoints), I see that the code enters vPortSuppressTicksAndSleep function.

/* Sleep until something happens. configPRE_SLEEP_PROCESSING() can set its parameter to 0 to indicate that its implementation contains its own wait for interrupt or wait for event instruction, and so wfi should not be executed again. However, the original expected idle time variable must remain unmodified, so a copy is taken. */
xModifiableIdleTime = xExpectedIdleTime;
configPRE_SLEEP_PROCESSING( xModifiableIdleTime );
if( xModifiableIdleTime > 0 )
{
 __asm volatile( "dsb" ::: "memory" );
 __asm volatile( "wfi" );
 __asm volatile( "isb" );
}
configPOST_SLEEP_PROCESSING( xExpectedIdleTime );

I also see that xExpectedIdleTime has a valid value. But after configPRE_SLEEP_PROCESSING( xModifiableIdleTime ); xModifiableIdleTime becomes 0 and it doesn't enter if( xModifiableIdleTime > 0 ) condition. Also the comment above mentioning "configPRE_SLEEP_PROCESSING() can

set its parameter to 0 to indicate that its implementation contains

its own wait for interrupt or wait for event instruction, and so wfi

should not be executed again." is confusing me.

Can someone shed some light on this?

This topic has been closed for replies.