Skip to main content
paolog
Associate III
Aug 9, 2023 9:42 AM UTC
Question

ThreadX scheduler in low power mode

Hi everyone.

I'm currently testing low power modes in ThreadX on a NUCLEO-F767ZI board using CubeMX and CubeIDE (current versions).

ThreadX tick period is set to 1 ms, and low power is enabled. What happens is that the scheduler awakes every millisecond even if HAL_SuspendTick() is called (seems because ThreadX SysTick_Handler remains active).

Shouldn't the scheduler be suspended for some milliseconds until next timer should be ready to run (or an interrupt would fire)? If this is correct a timeout timer seems to be not necessary. Is this due to the faster ThreadX tick?

This is the partial code:

 

 

void App_ThreadX_LowPower_Enter(void)
{
 /* USER CODE BEGIN App_ThreadX_LowPower_Enter */
 HAL_SuspendTick();

 HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
 /* USER CODE END App_ThreadX_LowPower_Enter */
}

void App_ThreadX_LowPower_Exit(void)
{
 /* USER CODE BEGIN App_ThreadX_LowPower_Exit */
 HAL_ResumeTick();
 /* USER CODE END App_ThreadX_LowPower_Exit */
}

ULONG App_ThreadX_TimerAdjust(void)
{
 /* USER CODE BEGIN App_ThreadX_TimerAdjust */
 uint32_t tmp1;

 tmp1 = __HAL_TIM_GET_COUNTER(&htim13);

 HAL_TIM_Base_Stop(&htim13);
 
 // Convert to system ticks, always returns 0 as timer is stopped in 1 ms
 return tmp1 / 1000;
 /* USER CODE END App_ThreadX_TimerAdjust */
}

void App_ThreadX_Timer_Setup(ULONG count)
{
 /* USER CODE BEGIN App_ThreadX_Timer_Setup */
 uint16_t timeout;

 timeout = (count * 1000 / TX_TIMER_TICKS_PER_SECOND);

 __HAL_TIM_SET_COUNTER(&htim13, 0);

 htim13.Instance->ARR = timeout * 1000 - 1;

 if (HAL_TIM_Base_Start(&htim13) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE END App_ThreadX_Timer_Setup */
}

 

 

Also, in order to reduce power consumption in sleep mode, is it correct to call __HAL_RCC_xxx_CLK_SLEEP_DISABLE once for the peripherals not needed in sleep mode?

Thank you for your comments.

 

This topic has been closed for replies.

2 replies

rdot
Graduate
Jun 11, 2024 10:20 PM UTC

@paolog Did you ever get an answer to this? I have the same questions on a STM32U5 project.

paolog
paologAuthor
Associate III
Jun 12, 2024 7:14 AM UTC

@rdot unfortunately not. So I decided to abandon ThreadX as no support is available. I moved to FreeRTOS (considering adopting SafeRTOS at a later project stage) as there's a lot more information available, as well examples.