Skip to main content
Associate III
Nov 26, 2024 12:12 AM UTC
Solved

Threadx On-the-fly update

Hello, 


I'm trying to find more information regarding ThreadX's on-the-fly properties update feature. In the ST Wiki article, there is mention of this feature, but none of the links and webpages seem to provide any details regarding what this feature is or how to use it. 

Introduction to THREADX - stm32mcu

 

Is the on the fly update the same as 'over the air' updates? Are there any articles about this feature? Have there been any coding examples showing how this feature is implemented?

Thanks

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Nov 26, 2024 12:47 AM UTC

It looks like "on-the-fly" refers to ability to update parts of running system. If so, this is based on the "modules" feature. You can download update to some module, swap it in and run without rebooting whole system. Like it was in the old good VxWorks.

Of course various settings can be changed in runtime, such as network parameters, IP address, keys and certificates, power management parameters etc.

 

 

1 reply

Pavel A.
Pavel A.Best answer
Nov 26, 2024 12:47 AM UTC

It looks like "on-the-fly" refers to ability to update parts of running system. If so, this is based on the "modules" feature. You can download update to some module, swap it in and run without rebooting whole system. Like it was in the old good VxWorks.

Of course various settings can be changed in runtime, such as network parameters, IP address, keys and certificates, power management parameters etc.