Skip to main content
MSipo
Senior II
March 26, 2021
Question

There is a bug in stm32l1xx_hal_conf.h. The MSI_VALUE value is wrong.

DeviceId = STM32L151RETx

FirmwarePackage = STM32Cube FW_L1 V1.10.2

Bug in: stm32l1xx_hal_conf.h

On row 110. The MSI_VALUE is defined as 16000000. It should be defined as 2097152 Hz

/**
 * @brief Internal Multiple Speed oscillator (MSI) default value.
 * This value is the default MSI range value after Reset.
 */
#if !defined (MSI_VALUE)
 #define MSI_VALUE ((uint32_t)16000000) /*!< Value of the Internal oscillator in Hz*/
#endif /* MSI_VALUE */

This topic has been closed for replies.

2 replies

ST Technical Moderator
March 26, 2021

Hello @Community member​ ,

I found different define in the latest firmware package that you may want to check out:

/**
 * @brief Internal Multiple Speed oscillator (MSI) default value.
 * This value is the default MSI range value after Reset.
 */
#if !defined (MSI_VALUE)
#define MSI_VALUE (2097000U) /*!< Value of the Internal oscillator in Hz*/
#endif /* MSI_VALUE */
 

Please make sure to use the latest release of STM32CubeL1 V1.10.2, then keep me infomed about your update.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
March 30, 2021

Hi @Community member​ ,

After check, it seems the error is in the template stm32l1xx_hal_conf.h when using CubeMX tool, which is not aligned with the HAL package.

 #if !defined (MSI_VALUE)
 #define MSI_VALUE ((uint32_t)16000000) /*!< Value of the Internal oscillator in Hz*/
#endif /* MSI_VALUE */
 

I have passed your feedback along to our CubeMX team for fix.

Thank you for bringing this issue to our attention.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks