Skip to main content
Miguel Moran
Associate II
May 15, 2023 6:01 PM UTC
Solved

The USB MSC Host library of FW_F7_V_17.1 in STM32F746-DISCOVERY does not work completely. Can you help me?

I was working with an example of the FW_F7_V_16.1 version and it works perfectly. When upgrading to version 17.1 I get an error "Error: Cannot Open USBHost.txt".

Checking a bit I found that the difference is mainly in the files:

usb_ctlreq.h and usbclreq.c

I suspect the ParseCfgDesc & ParseEPDesc functions.

However there are details I don't understand and I couldn't find out more.

Searching in the community I found the link to update the version and coincidentally the above mentioned files, where an update is mentioned

STM32F746-DISCOVERY. USB HOST FS MSC not working. Application state never go to state "APPLICATION READY"

We confirm the issue that is in USB Host library V3.4.1 and that was fixed in V3.5.0.

STM32F7 CubeFW release still doesn't integrate USB Host V3.5.0, but you can get it here on GitHub and use it in your package to fix the problem.

Future updates of STM32F7 package will contain V3.5.1.

However I downloaded it and updated it in my project and the problem was corrected "I can now write the file". 

The problem now is that when viewing the USB drive directory I see files that were never created.

This topic has been closed for replies.
Miguel Moran
Miguel MoranBest answer
Associate II
Jun 29, 2023 12:52 AM UTC

I understand the effort made with the updates, but being cautious I will stay with the previous version V2.6.0 and we will try the new versions v3.5.0 and v3.5.1 later on.

Thank you!!!

2 replies

ABOUA
ST Employee
May 24, 2023 4:19 PM UTC

Hello Miguel,

we highly recommend you to use host lib v3.5.0 or v3.5.1

did you check with already provided project on the cubeFW?

could you please start with formatted USB driver?

Regards,

Miguel Moran
Miguel MoranAuthorBest answer
Associate II
Jun 29, 2023 12:52 AM UTC

I understand the effort made with the updates, but being cautious I will stay with the previous version V2.6.0 and we will try the new versions v3.5.0 and v3.5.1 later on.

Thank you!!!