Skip to main content
Visitor II
Nov 8, 2023 9:44 AM UTC
Question

The ST-LINK_gdbserver has consistently been stalled in a state of awaiting linkage

 
  • Issue
Debugging is functional when employing the IDE; however, when utilizing the Command Line Interface approach, it invariably remains in a state of connection anticipation.
  • CMD:
ST-LINK_gdbserver -d -v -t -cp /opt/ST/STM32CubeCLT/STM32CubeProgrammer/bin/ -s -k -f /Users/pymcu/micropython/log.log
 
  • Log info:
[0.000] initConfigParams():  Configuration flags start
[0.000] initConfigParams():   external-init                  false
[0.000] initConfigParams():   pend-halt-timeout              (null)
[0.000] initConfigParams():   halt                           false
[0.000] initConfigParams():   config-file                    ""
[0.000] initConfigParams():   persistent                     false
[0.000] initConfigParams():  +log-file                       "/Users/pymcu/micropython/log.log"
[0.000] initConfigParams():   log-level                      31
[0.000] initConfigParams():   port-number                    61234
[0.000] initConfigParams():  +verbose                        true
[0.000] initConfigParams():   refresh-delay                  15
[0.000] initConfigParams():  +verify                         true
[0.000] initConfigParams():  +swd                            true
[0.000] initConfigParams():   swo-port                       61234
[0.000] initConfigParams():   cpu-clock                      8000000
[0.000] initConfigParams():   swo-clock-div                  128
[0.000] initConfigParams():  +initialize-reset               true
[0.000] initConfigParams():   debuggers                      false
[0.000] initConfigParams():   serial-number                  ""
[0.000] initConfigParams():   apid                           0
[0.000] initConfigParams():   attach                         false
[0.000] initConfigParams():  +shared                         true
[0.000] initConfigParams():   erase-all                      false
[0.000] initConfigParams():   memory-map                     ""
[0.000] initConfigParams():   ext-memory-loaders             false
[0.000] initConfigParams():   extload_init                   (null)
[0.000] initConfigParams():   extload                        (null)
[0.000] initConfigParams():  +stm32cubeprogrammer-path       "/opt/ST/STM32CubeCLT/STM32CubeProgrammer/bin/"
[0.000] initConfigParams():   temp-path                      ""
[0.000] initConfigParams():   preserve-temps                 false
[0.000] initConfigParams():   frequency                      0
[0.000] initConfigParams():   licenses                       false
[0.000] initConfigParams():   ignore-rest                    false
[0.000] initConfigParams():   version                        false
[0.000] initConfigParams():   help                           false
[0.000] initConfigParams():  Configuration flags end
[0.000] init():  STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
[0.118] openDevice():  COM frequency = 4000 kHz
[0.118] openDevice():  Target connection mode: Under reset
[0.128] readFromTarget():  Reading ROM table for AP 0 @0xe00fdfd0
[0.132] reset_hw_wtchpt_module():  Hardware watchpoint supported by the target
[0.138] initContext():  ST-LINK Firmware version : V2J42M27
[0.138] initContext():  Device ID: 0x451
[0.139] initContext():  PC: 0x8002f8c
[0.139] Device_GetStatus():  ST-LINK device status: HALT_MODE
[0.140] initContext():  ST-LINK detects target voltage = 3.26 V
[0.140] initContext():  ST-LINK device status: HALT_MODE
[0.140] initServerContext():  ST-LINK device initialization OK
[0.140] pollAndNotifyRun():  Stm32Device, pollAndNotify running...
[0.141] updateState():  SwvSrv state change: 0 -> 1
[0.141] WaitConnection():  Waiting for connection on port 61235...
[0.141] WaitConnection():  Waiting for connection on port 61234...
This topic has been closed for replies.