Skip to main content
Associate
July 14, 2026
Solved

The software project about STM32G473cbt6 and STM32G474cbt6

Hi ST expert

STM32G473cbt6 and STM32G474cbt6 are pin-to-pin compatible, can their software projects be designed into one project?

MOBEJ
MOBEJBest answer
ST Employee
July 14, 2026

Hello ​@licunxu  ,

Yes. STM32G474 is basically STM32G473 + an HRTIM1 timer — everything else (ADCs, DACs, comparators, op-amps, communication peripherals, Flash/RAM) is the same, and since your packages are pin-to-pin compatible, one project can serve both.

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

MOBEJ
MOBEJBest answer
ST Employee
July 14, 2026

Hello ​@licunxu  ,

Yes. STM32G474 is basically STM32G473 + an HRTIM1 timer — everything else (ADCs, DACs, comparators, op-amps, communication peripherals, Flash/RAM) is the same, and since your packages are pin-to-pin compatible, one project can serve both.

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
licunxuAuthor
Associate
July 23, 2026

Hello MOBEJ

       Thank you for your reply!