Skip to main content
PChau.1
Associate II
Apr 2, 2022 9:51 PM UTC
Question

The LED screen on the BL4622ECell1 that I bought has stopped working, WHY?

The BL462ECELL1 that I bought, I have been working on it for the last 5 days. I was wandering around in search of the answer for how to get the module sim registered as the registration past was getting denied over and over again. I have already activated the sim, but I am now struggling with the registration process and the turned-off LED screen on the module,

I seek desperate help from the ST team.

Thank you

This topic has been closed for replies.

10 replies

MM..1
Super User
Apr 3, 2022 11:42 AM UTC

Stopped ? Or never work on? Your description isnt clean. Load ready to go example code ...

PChau.1
PChau.1Author
Associate II
Apr 4, 2022 12:23 AM UTC

it was working earlier. but now it's just turned off. where could i find this ready to go example code

PChau.1
PChau.1Author
Associate II
Apr 4, 2022 12:27 AM UTC

  ATParser:*** SEND (size=9) ***

AT%CEER?<CR>

  <CR><LF>

  %CEER: 1<CR><LF>

  <CR><LF>

  OK<CR><LF>

  ATParser:*** SEND (size=9) ***

AT+COPS?<CR>

  <CR><LF>

  +COPS: 0<CR><LF>

  <CR><LF>

  OK<CR><LF>

CST: CST_set_signal_quality

CST: osCS_get_signal_quality()

  ATParser:*** SEND (size=7) ***

AT+CSQ<CR>

  <CR><LF>

  +CSQ: 99,99<CR><LF>

  <CR><LF>

  OK<CR><LF>

CST: Sig quality rssi : 99

CST: Sig quality ber : 99

CST: CST_send_message: POLLING_TIMER_EVENT

CST: AUTOM TASK: WAITING_FOR_NETWORK_STATUS_STATE - POLLING_TIMER_EVENT

CST: CST_network_status_test_mngt

CST: CST_get_network_status

CST: osCDS_get_net_status()

  ATParser:*** SEND (size=10) ***

AT+CEREG?<CR>

  <CR><LF>

  +CEREG: 2,2<CR><LF>

ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING

  <CR><LF>

  OK<CR><LF>

  ATParser:*** SEND (size=9) ***

AT+CREG?<CR>

  <CR><LF>

  +CREG: 2,0<CR><LF>

ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING

  <CR><LF>

  OK<CR><LF>

  ATParser:*** SEND (size=9) ***

AT%CEER?<CR>

  <CR><LF>

  %CEER: 1<CR><LF>

  <CR><LF>

  OK<CR><LF>

  ATParser:*** SEND (size=9) ***

AT+COPS?<CR>

  <CR><LF>

  +COPS: 0<CR><LF>

  <CR><LF>

  OK<CR><LF>

CST: CST_set_signal_quality

CST: osCS_get_signal_quality()

  ATParser:*** SEND (size=7) ***

AT+CSQ<CR>

  <CR><LF>

  +CSQ: 99,99<CR><LF>

  <CR><LF>

  OK<CR><LF>

CST: Sig quality rssi : 99

CST: Sig quality ber : 99

CST: CST_send_message: POLLING_TIMER_EVENT

CST: AUTOM TASK: WAITING_FOR_NETWORK_STATUS_STATE - POLLING_TIMER_EVENT

CST: CST_network_status_test_mngt

CST: CST_get_network_status

CST: osCDS_get_net_status()

  ATParser:*** SEND (size=10) ***

AT+CEREG?<CR>

  <CR><LF>

  +CEREG: 2,2<CR><LF>

ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING

  <CR><LF>

  OK<CR><LF>

  ATParser:*** SEND (size=9) ***

AT+CREG?<CR>

  <CR><LF>

  +CREG: 2,0<CR><LF>

ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING

  <CR><LF>

  OK<CR><LF>

  ATParser:*** SEND (size=9) ***

AT%CEER?<CR>

  <CR><LF>

  %CEER: 1<CR><LF>

  <CR><LF>

  OK<CR><LF>

  ATParser:*** SEND (size=9) ***

AT+COPS?<CR>

  <CR><LF>

  +COPS: 0<CR><LF>

  <CR><LF>

  OK<CR><LF>

this is what i am getting over and over again. suggest me something. i will be waiting for your reply

ST Technical Moderator
Apr 14, 2022 9:01 AM UTC

Hello @PChau.1​ and welcome to the Community :)

This is not my area of expertise, but I added the topic X-Cube-Cellular to your question in order to increase its chance to be reviewed by our experts.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
PChau.1
PChau.1Author
Associate II
Apr 14, 2022 2:12 PM UTC

Thankyou Imen for your support.:smiling_face_with_smiling_eyes:​

PChau.1
PChau.1Author
Associate II
Apr 14, 2022 2:19 PM UTC

Imen, it would mean a lot to me if you could suggest me any names, those who can help me​ solve my problem.

S.RA
ST Employee
Apr 21, 2022 11:43 AM UTC

Dear PChau.1,

Please can you provide a complete log, start from the device startup just to understand the overall behaviour. In fact, based on what you share, it looks that the device did not find any network.

please record the log from the terminal and share it for further analysis.

Thanks

Best Regards

Solofo

PChau.1
PChau.1Author
Associate II
Apr 21, 2022 6:26 PM UTC

These two files contain the recording of the terminal, and the problem I face, I hope to get a solution,

with high hopes

PChau.1

PChau.1
PChau.1Author
Associate II
Apr 21, 2022 6:27 PM UTC

suggest mew what should I do to get the sim registered

PChau.1

Visitor II
Mar 28, 2024 4:37 PM UTC

I am facing the same issue with the BL462 CELL1 Board. The OLED suddenly turned off after being registered with an esim and running an example code provided by X-CUBE CELLULAR.  And it's not been working since then. 

 

Immediate help from Pchau.1 or ST team would be greatly appreciated.

Thanks in advance