Solved
Test device network speed
- April 26, 2024
- 5 replies
- 3569 views
Hi guys,
I want to know whether the device meets the 100Mbps full duplex need how to test?
My own test is as follows:
The device ip is 192.168.1.10, pc ip is 192.168.1.135.(The ip of pc is different in wireshark(135) and test software(25), because it is not the same pc and same test, just for your information)
First of all, when connecting the device to PC via RJ45, the Ethernet link shows 100Mbps. I used the speed test software on PC, when sending arp, icmp, tcp, udp packets to the device at the same time, the device won't reply to some of the packets, especially not to ICMP packets.
In this case, is the device considered to meet the 100 megabit full duplex? Or do all requests have to be replied by the device.