Skip to main content
Mujtaba
Associate III
May 10, 2020 11:40 AM UTC
Solved

TCP Server & Client, lwIP Netconn API

Dear friends,

I am trying to establish a robust TCP interaction between two different boards with the same MCU (stm32f407vgt6) and ethernet phy (dp83848cvv) and I use lwIP Netconn APIs as TCP/IP stack and freeRTOS as a real time operating system.

In both MCUs I must run a TCP server task and a TCP Client task. When both boards are connected together directly there is no problem. The problem occurs when both boards are connected through a network switch. After working for a while, the boards TCP tasks (Server & Client) stop working and the boards do not ping. (Ping request is timed out.)

The code for Server and Client tasks are as bellow:

void Task_TCP_Server(void const * argument)
{
 /* init code for LWIP */
 MX_LWIP_Init();
 
 /* USER CODE BEGIN 5 */
	
	struct netconn *conn, *newconn;
 err_t err, accept_err;
 struct netbuf *buf;
 void *data;
 u16_t len;
 err_t recv_err;
 uint8_t *tcp_rx_buf; 
	uint8_t temp_buff[100] = {0};
	data_type respond_len = {0};
	data_type start_addr = {0};
	data_type num_reg = {0};
	uint8_t byte_cnt = 0;
	
 LWIP_UNUSED_ARG(argument);
 
//	osDelay(50);
 /* Create a new connection identifier. */
 conn = netconn_new(NETCONN_TCP);
 
 if (conn!=NULL)
 { 
 /* Bind connection to well known port number 7. */
 err = netconn_bind(conn, NULL, TCP_SERVER_PORT_NUMBER);
 
 if (err == ERR_OK)
 {
 /* Tell connection to go into listening mode. */
 netconn_listen(conn);
 
 while (1) 
 {
 /* Grab new connection. */
 accept_err = netconn_accept(conn, &newconn);
 
 /* Process the new connection. */
 if (accept_err == ERR_OK) 
 {
 recv_err = netconn_recv(newconn, &buf);
					while ( recv_err == ERR_OK) 
 {
 do 
 {
 netbuf_data(buf, &data, &len);
							
							tcp_rx_buf = (uint8_t *)data;
							
							if(tcp_rx_buf[2] == 0x00 && tcp_rx_buf[3] == 0x00)
							{
								/* Transaction ID */
								temp_buff[0] = tcp_rx_buf[0];
								temp_buff[1] = tcp_rx_buf[1];
								
								/* Protocol ID */
								temp_buff[2] = tcp_rx_buf[2];
								temp_buff[3] = tcp_rx_buf[3];
																
								/* Unit Identifier */
								temp_buff[6] = tcp_rx_buf[6];
								
							
								start_addr.byte[1] = tcp_rx_buf[8];
								start_addr.byte[0] = tcp_rx_buf[9];
								
								if(tcp_rx_buf[7] == PRESET_MULTIPLE_REG_FCODE)
								{
									
									num_reg.byte[1] = tcp_rx_buf[10];
									num_reg.byte[0] = tcp_rx_buf[11];
									
									byte_cnt = tcp_rx_buf[12];
									
									if(tcp_rx_buf[14] == ON)
										Relay_Write(RELAY_CHANNEL_1, MH_RELAY_ON);
									
									else
										Relay_Write(RELAY_CHANNEL_1, MH_RELAY_OFF);
																		
									if(tcp_rx_buf[16] == ON)
										Relay_Write(RELAY_CHANNEL_2, MH_RELAY_ON);
									
									else
										Relay_Write(RELAY_CHANNEL_2, MH_RELAY_OFF);
																		
									if(tcp_rx_buf[18] == ON)
										Relay_Write(RELAY_CHANNEL_3, MH_RELAY_ON);
									
									else
										Relay_Write(RELAY_CHANNEL_3, MH_RELAY_OFF);
																		
									if(tcp_rx_buf[20] == ON)
										Relay_Write(RELAY_CHANNEL_4, MH_RELAY_ON);
									
									else
										Relay_Write(RELAY_CHANNEL_4, MH_RELAY_OFF);
																		
									if(tcp_rx_buf[22] == ON)
										Relay_Write(RELAY_CHANNEL_5, MH_RELAY_ON);
									
									else
										Relay_Write(RELAY_CHANNEL_5, MH_RELAY_OFF);
																		
									if(tcp_rx_buf[24] == ON)
										Relay_Write(RELAY_CHANNEL_6, MH_RELAY_ON);
									
									else
										Relay_Write(RELAY_CHANNEL_6, MH_RELAY_OFF);
																		
									if(tcp_rx_buf[26] == ON)
										Relay_Write(RELAY_CHANNEL_7, MH_RELAY_ON);
									
									else
										Relay_Write(RELAY_CHANNEL_7, MH_RELAY_OFF);
																		
									if(tcp_rx_buf[28] == ON)
										Relay_Write(RELAY_CHANNEL_8, MH_RELAY_ON);
									
									else
										Relay_Write(RELAY_CHANNEL_8, MH_RELAY_OFF);
																		
									netconn_write(newconn, data, len, NETCONN_COPY);
									
								}
								
//								else if(tcp_rx_buf[7] == PRESET_SINGLE_REG_FCODE)
//								{
//									
//									Write_Group_SingleReg_TCP(start_addr.value);
//									netconn_write(newconn, data, len, NETCONN_COPY);
//									
//								}
									
								else
								{
									netconn_write(newconn, data, len, NETCONN_COPY);	
								}
							}
							
							else
							{
							 netconn_write(newconn, data, len, NETCONN_COPY);	
							}
 
 } 
 while (netbuf_next(buf) >= 0);
 
 netbuf_delete(buf);
						recv_err = netconn_recv(newconn, &buf);
 }
 
 /* Close connection and discard connection identifier. */
 netconn_close(newconn);
 netconn_delete(newconn);
 }
 }
 }
 else
 {
 netconn_delete(newconn);
 printf(" can not bind TCP netconn");
 }
 }
 else
 {
 printf("can not create TCP netconn");
 }
	
 /* USER CODE END 5 */ 
}
void Task_TCP_Client(void const * argument)
{
 
 
 /* USER CODE BEGIN 5 */
	
	uint8_t pData[10] = {0};
	osEvent evt;
	err_t err;
	ip4_addr_t serverIPAddress;
	struct netbuf *recvData;
	char *dataBuff;
 
	osDelay(300);
	
	IP4_ADDR(&serverIPAddress, SERVER_IP_0, SERVER_IP_1, SERVER_IP_2, SERVER_IP_3);
 
		
	while(1)
	{
		osSignalWait(0x01, osWaitForever);
			
			struct netconn* tcpClientConn = netconn_new(NETCONN_TCP);
 
			if(tcpClientConn != NULL)
			{
								
				if(err == ERR_OK)
				{
												
						err = netconn_connect(tcpClientConn, &serverIPAddress, 503);
						
						if(err == ERR_OK)
						{
							
							err = netconn_write(tcpClientConn, &sendData[1], sendData[0], NETCONN_COPY);
							
							if(err == ERR_OK)
							{
								
								err = netconn_recv(tcpClientConn, &recvData);
								
								if(err == ERR_OK)
								{
									
									netbuf_data(recvData, (void *)&dataBuff, &netbuf_len(recvData));
									
									
									netbuf_delete(recvData);
									
									err = netconn_close(tcpClientConn);
									
									if(err == ERR_OK)
									{
									}
									
									err = netconn_delete(tcpClientConn);
									
									if(err == ERR_OK)
									{
									}
								}
								
								else
								{
									netconn_close(tcpClientConn);
									
									
									err = netconn_delete(tcpClientConn);
									
									if(err == ERR_OK)
									{
									}
									
								}
								
							}
							
							else
							{
								err = netconn_close(tcpClientConn);
								
								if(err == ERR_OK)
								{
								}
								
								
								err = netconn_delete(tcpClientConn);
								
								if(err == ERR_OK)
								{
								}
							}
						}
						
					
						else
						{
							err = netconn_delete(tcpClientConn);
							
							if(err == ERR_OK)
							{
							}
						}
					
				}	
 
				
				else
				{
					netconn_delete(tcpClientConn);
				}			
				
				
			}
			
			else
			{
			}
		
	}
 /* USER CODE END 5 */ 
}

Any helps would be appreciated in advance,

kind regards,

Mujtaba

This topic has been closed for replies.
Mujtaba
MujtabaBest answer
Associate III
May 14, 2020 1:04 PM UTC

Hello Kurta,

the problem was in the MAC address. I forgot to change the MAC address of two boards.

2 replies

kurta999
Senior
May 10, 2020 11:50 AM UTC

Hi,

After working for a while -> how long does it work for you? We also experiencing with LwIP and for us it was stable for 2 days without any problems, I haven't tested it longer yet.

Mujtaba
MujtabaAuthorBest answer
Associate III
May 14, 2020 1:04 PM UTC

Hello Kurta,

the problem was in the MAC address. I forgot to change the MAC address of two boards.