Skip to main content
Necrotos
Associate
Jan 6, 2023 11:43 PM UTC
Question

TCP Client on NUCLEO-F746ZG can't connect to a TCP Server on my PC using Hercules

Hello,

I want to transmit data between two boards using TCP. To do this, one will run a client and the other will run a server. Both of these implementations follow the provided examples. The server works fine, I can connect to it from Hercules and transfer data.

The client implementation is causing me problems, as it can't seem to establish a connection to a TCP server. I can however ping it just fine. Both boards are assigned an IP via DHCP, but the address is always the same and matches with what I expect. Here is the code:

static void tcpecho_client_thread(void const *arg)
{
 struct netconn *xNetConn = NULL;
 
 err_t bind_err, connect_err;
 
 char* b_data = "OK"; // Data to be sent
 uint16_t b_len = sizeof ( b_data );
 
 IP4_ADDR(&local_ip, IP_ADDR0_CLIENT, IP_ADDR1_CLIENT, IP_ADDR2_CLIENT, IP_ADDR3_CLIENT);
 IP4_ADDR(&pc_ip, IP_ADDR0_PC, IP_ADDR0_PC, IP_ADDR2_PC, IP_ADDR3_PC);
 
 xNetConn = netconn_new ( NETCONN_TCP );
 if (xNetConn != NULL){
 bind_err = netconn_bind ( xNetConn, &local_ip, TCP_PORT_NETCONN );
 
 if(bind_err == ERR_OK){
 
 // Try to connect to server
 for(;;){
 connect_err = netconn_connect ( xNetConn, &pc_ip, TCP_PORT_NETCONN);
 
 if (connect_err == ERR_OK){
 // We are connected
 while(1){
 BSP_LED_On(LED1);
 netconn_write(xNetConn, b_data, b_len, NETCONN_COPY);
 vTaskDelay(1000); // To see the result easily in Comm Operator
 }
 }
 }
 }else{
 // Failed to bind the connection
 BSP_LED_On(LED3);
 }
 }else{
 // Failed to allocate a new connection
 BSP_LED_On(LED3);
 }
 
}

As I can ping it, I don't think something is fundamentally wrong. Is there something I am missing here? In the for loop, it should try to establish a connection until it succeeds, but it never actually manages to connect to something.

This topic has been closed for replies.

5 replies

Pavel A.
Jan 7, 2023 12:20 AM UTC

Is the server a Windows PC? Firewall enabled?

Necrotos
NecrotosAuthor
Associate
Jan 7, 2023 12:29 AM UTC

I have tried with the server on my Windows PC using Hercules. In that there should be at least the default Windows Firewall (at least to my knowledge).

I have also tried running a simple server on a second board. In that case, both are in the same subnet so the Firewall shouldn't play a role in that case.

Pavel A.
Jan 7, 2023 4:34 AM UTC

Well, then it's the time for wireshark.