Skip to main content
Associate
Feb 14, 2025 5:16 PM UTC
Question

SysTick not incrementing with TrustZone enabled

I have a simple project set up for the stm32h573II-DK that has USART1 set up and I can print to serial out over the same USB connector that uses ST-LINK with HAL_UART_Transmit(&hcom_uart[COM1], MSG, sizeof(MSG), 100);. I can not use HAL_Delay(1000); to print every ~1 second. When entering the HAL_Delay function, I can see with a debugger that uwTick is never incremented and with breakpoints I can see that the systick handler is never called. I made a project that doesn't have TrustZone set up and it can print every one second. I do not think this is an ISR priority issue, as I am calling HAL_Delay() from main(). All of the code was generated with cubemx and the only edits I've made were to add the print. What could I be doing wrong to prevent the systick interrupt from being handled correctly?

This topic has been closed for replies.

1 reply

ST Employee
Apr 3, 2025 1:58 PM UTC

Hello @chipchop, 

The SysTick timer is used as the timebase in the default HAL implementation, is this issue within an RTOS context? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.