Skip to main content
'SMike
Associate III
Aug 30, 2022 2:49 PM UTC
Solved

SysTick does not update during init

If Azure ThreadX is enabled, Systick no longer updates; HAL_IncTick() is no longer called from the interrupt, and initialization fails.

This topic has been closed for replies.
'SMike
'SMikeBest answer
Associate III
Aug 31, 2022 3:05 PM UTC

I was able to fix this and move forward.

So ThreadX "steals" the SysTick interrupt from the HAL. The priorities seem fine. But the HAL interrupt handler calls HAL_IncTick, and when ThreadX is enabled, it no longer gets called (ThreadX has it's own version of SysTick interrupt handler). So I enabled TIM2. You have to move the init code for TIM2 above the rest of the HAL init:

/* USER CODE END Boot_Mode_Sequence_2 */
 
 /* USER CODE BEGIN SysInit */
 
	MX_TIM2_Init(); // timer must be started before using HAL, it replaces SysTick
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DSIHOST_DSI_Init();
 MX_FMC_Init();

and start the timer in MX_TIM2_Init():

 /* USER CODE BEGIN TIM2_Init 2 */
 
 HAL_TIM_Base_Start_IT(&htim2); // Enable the interrupt & start the timer
 /* USER CODE END TIM2_Init 2 *

then call the SysTick function from the interrupt:

void TIM2_IRQHandler(void)
{
 /* USER CODE BEGIN TIM2_IRQn 0 */
 
 /* USER CODE END TIM2_IRQn 0 */
 HAL_TIM_IRQHandler(&htim2);
 /* USER CODE BEGIN TIM2_IRQn 1 */
 
 HAL_IncTick();	// Need to emulate the SysTick to enable HAL initialization
 /* USER CODE END TIM2_IRQn 1 */
}

HTH someone...

3 replies

Javier1
Principal
Aug 31, 2022 9:43 AM UTC

check your NVIC preemption

HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);

and your systick priority

HAL_InitTick(TICK_INT_PRIORITY);

speciall atention to this part inside HAL_InitTick

/* Configure the SysTick IRQ priority */
 if (TickPriority < (1UL << __NVIC_PRIO_BITS))
 {
 HAL_NVIC_SetPriority(SysTick_IRQn, TickPriority, 0U);
 uwTickPrio = TickPriority;
 }
 else
 {
 return HAL_ERROR;
 }

, there is a good chance threadX NVIC setup is bullying your systick interruption setup.

hit me up in https://www.linkedin.com/in/javiermuñoz/
'SMike
'SMikeAuthorBest answer
Associate III
Aug 31, 2022 3:05 PM UTC

I was able to fix this and move forward.

So ThreadX "steals" the SysTick interrupt from the HAL. The priorities seem fine. But the HAL interrupt handler calls HAL_IncTick, and when ThreadX is enabled, it no longer gets called (ThreadX has it's own version of SysTick interrupt handler). So I enabled TIM2. You have to move the init code for TIM2 above the rest of the HAL init:

/* USER CODE END Boot_Mode_Sequence_2 */
 
 /* USER CODE BEGIN SysInit */
 
	MX_TIM2_Init(); // timer must be started before using HAL, it replaces SysTick
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DSIHOST_DSI_Init();
 MX_FMC_Init();

and start the timer in MX_TIM2_Init():

 /* USER CODE BEGIN TIM2_Init 2 */
 
 HAL_TIM_Base_Start_IT(&htim2); // Enable the interrupt & start the timer
 /* USER CODE END TIM2_Init 2 *

then call the SysTick function from the interrupt:

void TIM2_IRQHandler(void)
{
 /* USER CODE BEGIN TIM2_IRQn 0 */
 
 /* USER CODE END TIM2_IRQn 0 */
 HAL_TIM_IRQHandler(&htim2);
 /* USER CODE BEGIN TIM2_IRQn 1 */
 
 HAL_IncTick();	// Need to emulate the SysTick to enable HAL initialization
 /* USER CODE END TIM2_IRQn 1 */
}

HTH someone...

Javier1
Principal
Sep 1, 2022 7:34 AM UTC

youre the best answer then! congrats

hit me up in https://www.linkedin.com/in/javiermuñoz/