Skip to main content
Senior
Feb 6, 2026 6:55 AM UTC
Solved

SysTick Callback not being generated?

Hi,

I am using a STM32C031G6U6 and I would appreciate some clarification regarding HAL timebase and SysTick timebase selection.

I want to use SysTick as a 1ms interrupt so in CubeMX I selected SysTick as timebase (see screenshot):

Ricko_0-1770359921026.png

 

None of the other timers - including TIM3 - are not enabled as shown here:

Ricko_1-1770360000600.png

 

These are the other settings:

Ricko_1-1770361629621.png

 

Ricko_0-1770361610071.png

 

I then generated the code. 

But there is no sign of any SysTick related functions/handlers in the interrupt file stm32c0xx_it.c as you can see here:

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file stm32c0xx_it.c
 * @brief Interrupt Service Routines.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2026 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32c0xx_it.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */


/******************************************************************************/
/* Cortex Processor Interruption and Exception Handlers */
/******************************************************************************/
/**
 * @brief This function handles Non maskable interrupt.
 */
void NMI_Handler(void)
{
 /* USER CODE BEGIN NonMaskableInt_IRQn 0 */

 /* USER CODE END NonMaskableInt_IRQn 0 */
 /* USER CODE BEGIN NonMaskableInt_IRQn 1 */
 while (1)
 {
 }
 /* USER CODE END NonMaskableInt_IRQn 1 */
}

/**
 * @brief This function handles Hard fault interrupt.
 */
void HardFault_Handler(void)
{
 /* USER CODE BEGIN HardFault_IRQn 0 */

 /* USER CODE END HardFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_HardFault_IRQn 0 */
 /* USER CODE END W1_HardFault_IRQn 0 */
 }
}

 

 

On the other hand it does seem that TIM3 is somehow used/generated in the generated code in the file  stm32c0xx_hal_timebase_tim_template.c  (see below).

 

/**
 ******************************************************************************
 * @file stm32c0xx_hal_timebase_tim_template.c
 * @author MCD Application Team
 * @brief HAL time base based on the hardware TIM.
 *
 * This file overrides the native HAL time base functions (defined as weak)
 * the TIM time base:
 * + Initializes the TIM peripheral to generate a Period elapsed Event each 1ms
 * + HAL_IncTick is called inside HAL_TIM_PeriodElapsedCallback ie each 1ms
 *
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2022 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 @verbatim
 ==============================================================================
 ##### How to use this driver #####
 ==============================================================================
 [..]
 This file must be copied to the application folder and modified as follows:
 (#) Rename it to 'stm32c0xx_hal_timebase_tim.c'
 (#) Add this file and the TIM HAL drivers to your project and uncomment
 HAL_TIM_MODULE_ENABLED define in stm32c0xx_hal_conf.h

 @endverbatim
 ******************************************************************************
 */

/* Includes ------------------------------------------------------------------*/
#include "stm32c0xx_hal.h"

/** @addtogroup STM32C0xx_HAL_Driver
 * @{
 */

/** @addtogroup HAL_TimeBase_TIM
 * @{
 */

/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
extern TIM_HandleTypeDef TimHandle;
TIM_HandleTypeDef TimHandle;
/* Private function prototypes -----------------------------------------------*/
void TIM3_IRQHandler(void);
/* Private functions ---------------------------------------------------------*/

/**
 * @brief This function configures the TIM3 as a time base source.
 * The time source is configured to have 1ms time base with a dedicated
 * Tick interrupt priority.
 * @note This function is called automatically at the beginning of program after
 * reset by HAL_Init() or at any time when clock is configured, by HAL_RCC_ClockConfig().
 * TickPriority Tick interrupt priority.
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority)
{
 RCC_ClkInitTypeDef clkconfig;
 uint32_t uwTimclock;
 uint32_t uwAPB1Prescaler;
 uint32_t uwPrescalerValue;
 uint32_t pFLatency;

 /*Configure the TIM3 IRQ priority */
 HAL_NVIC_SetPriority(TIM3_IRQn, TickPriority, 0U);

 /* Enable the TIM3 global Interrupt */
 HAL_NVIC_EnableIRQ(TIM3_IRQn);

 /* Enable TIM3 clock */
 __HAL_RCC_TIM3_CLK_ENABLE();

 /* Get clock configuration */
 HAL_RCC_GetClockConfig(&clkconfig, &pFLatency);

 /* Get APB1 prescaler */
 uwAPB1Prescaler = clkconfig.APB1CLKDivider;

 /* Compute TIM3 clock */
 if (uwAPB1Prescaler == RCC_APB1_DIV1)
 {
 uwTimclock = HAL_RCC_GetPCLK1Freq();
 }
 else
 {
 uwTimclock = 2U * HAL_RCC_GetPCLK1Freq();
 }

 /* Compute the prescaler value to have TIM3 counter clock equal to 1MHz */
 uwPrescalerValue = (uint32_t)((uwTimclock / 1000000U) - 1U);

 /* Initialize TIM3 */
 TimHandle.Instance = TIM3;

 /* Initialize TIMx peripheral as follow:
 + Period = [(TIM3CLK/1000) - 1]. to have a (1/1000) s time base.
 + Prescaler = (uwTimclock/1000000 - 1) to have a 1MHz counter clock.
 + ClockDivision = 0
 + Counter direction = Up
 */
 TimHandle.Init.Period = (1000000U / 1000U) - 1U;
 TimHandle.Init.Prescaler = uwPrescalerValue;
 TimHandle.Init.ClockDivision = 0U;
 TimHandle.Init.CounterMode = TIM_COUNTERMODE_UP;
 TimHandle.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&TimHandle) == HAL_OK)
 {
 /* Start the TIM time Base generation in interrupt mode */
 return HAL_TIM_Base_Start_IT(&TimHandle);
 }

 /* Return function status */
 return HAL_ERROR;
}

/**
 * @brief Suspend Tick increment.
 * @note Disable the tick increment by disabling TIM3 update interrupt.
 * @retval None
 */
void HAL_SuspendTick(void)
{
 /* Disable TIM3 update interrupt */
 __HAL_TIM_DISABLE_IT(&TimHandle, TIM_IT_UPDATE);
}

/**
 * @brief Resume Tick increment.
 * @note Enable the tick increment by enabling TIM3 update interrupt.
 * @retval None
 */
void HAL_ResumeTick(void)
{
 /* Enable TIM3 update interrupt */
 __HAL_TIM_ENABLE_IT(&TimHandle, TIM_IT_UPDATE);
}

/**
 * @brief Period elapsed callback in non blocking mode
 * @note This function is called when TIM3 interrupt took place, inside
 * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
 * a global variable "uwTick" used as application time base.
 * htim TIM handle
 * @retval None
 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 HAL_IncTick();
}

/**
 * @brief This function handles TIM interrupt request.
 * @retval None
 */
void TIM3_IRQHandler(void)
{
 HAL_TIM_IRQHandler(&TimHandle);
}

/**
 * @}
 */

/**
 * @}
 */

 

 

What is happening? Am I looking in the wrong file?

Where is the SysTick handler in which I can plug my custom functions that I need to run every 1ms?

 

 

Thank you

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 6, 2026 11:38 AM UTC

@Ricko wrote:

Did you have to tick that manually?

Thank you


No. Just created a project from scratch and  it was already checked:

mALLEm_0-1770377843307.png

May be you've unchecked it by mistake.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

5 replies

Ozone
Principal
Feb 6, 2026 7:12 AM UTC

The handling of Systick is one of the reasons I dislike Cube/HAL and don't use it.

But as a pragmatic approach, you could do two thing to locate the Systick implementation.
The first is the mep file, it lists all functions linked in, their addresses, and the source file.
The second option is to look up the name of the SysTick handler in the startup code, and do a file search.

mƎALLEm
ST Technical Moderator
Feb 6, 2026 7:57 AM UTC

Hello,

I've just generated a code with CubeMx based on STM32C031G6U6 and the interrupt is located in stm32c0xx_it.c:

/******************************************************************************/
/* Cortex Processor Interruption and Exception Handlers */
/******************************************************************************/
/**
 * @brief This function handles Non maskable interrupt.
 */
void NMI_Handler(void)
{
 /* USER CODE BEGIN NonMaskableInt_IRQn 0 */

 /* USER CODE END NonMaskableInt_IRQn 0 */
 /* USER CODE BEGIN NonMaskableInt_IRQn 1 */
 while (1)
 {
 }
 /* USER CODE END NonMaskableInt_IRQn 1 */
}

/**
 * @brief This function handles Hard fault interrupt.
 */
void HardFault_Handler(void)
{
 /* USER CODE BEGIN HardFault_IRQn 0 */

 /* USER CODE END HardFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_HardFault_IRQn 0 */
 /* USER CODE END W1_HardFault_IRQn 0 */
 }
}

/**
 * @brief This function handles System service call via SWI instruction.
 */
void SVC_Handler(void)
{
 /* USER CODE BEGIN SVC_IRQn 0 */

 /* USER CODE END SVC_IRQn 0 */
 /* USER CODE BEGIN SVC_IRQn 1 */

 /* USER CODE END SVC_IRQn 1 */
}

/**
 * @brief This function handles Pendable request for system service.
 */
void PendSV_Handler(void)
{
 /* USER CODE BEGIN PendSV_IRQn 0 */

 /* USER CODE END PendSV_IRQn 0 */
 /* USER CODE BEGIN PendSV_IRQn 1 */

 /* USER CODE END PendSV_IRQn 1 */
}

/**
 * @brief This function handles System tick timer.
 */
void SysTick_Handler(void)
{
 /* USER CODE BEGIN SysTick_IRQn 0 */

 /* USER CODE END SysTick_IRQn 0 */
 HAL_IncTick();
 /* USER CODE BEGIN SysTick_IRQn 1 */

 /* USER CODE END SysTick_IRQn 1 */
}

When using Systick is used as time base for the HAL, the configuration is stm32c0xx_hal.c.

So what CubeMx version are you using? and could you please share your ioc file?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
RickoAuthor
Senior
Feb 6, 2026 11:31 AM UTC

Thank you @mƎALLEm 

I just noticed that - as you can see from my original screenshot - the checkbox below was not ticked.

Ricko_0-1770377396740.png

I have now ticked it and it generates it like in your uploaded code.

In the past I did not have to do that. So that's strange.

Did you have to tick that manually?

Thank you

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 6, 2026 11:38 AM UTC

@Ricko wrote:

Did you have to tick that manually?

Thank you


No. Just created a project from scratch and  it was already checked:

mALLEm_0-1770377843307.png

May be you've unchecked it by mistake.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
RickoAuthor
Senior
Feb 8, 2026 10:34 AM UTC

Thank you @mƎALLEm 

I dind't that why I was surprised it was not ticked. I think it might be because I enabled freeRTOS and generated the code then turned off freeeRTOS.

Thank you :smiling_face_with_smiling_eyes: