Skip to main content
hijax_pl
Associate III
Nov 27, 2024 12:35 PM UTC
Question

SVD for STM32H503, TIMx_SMCR inconsistency

(1) TIM1_SMCR and TIM2/3_SMCR have different naming convetions for SMS / TS fields

i.e. for TIM1_SMCR there are SMS/SMS_1 and TS/TS_1 and for TIM2/3_SMCR, SMS1/SMS2 and TS1/TS2 respectively.

(2) Also TIM1_SMCR_TS_1 field has no enumerated values, while for TIM2/3_SMCR_TS2 there are, but wrongly described. TIM1_SMCR_TS & TIM2/3_SMCR_TS1 has enums for the range 0..7 only, ie. the TS1 field itself.

As described in the RM0492, those fields must be combined.

I think the easies way forward would be to provide enums only for the TS1 field, and add missing values:

B_0x10000:Internal Trigger 4 (tim_itr4)
B_0x10001:Internal Trigger 5 (tim_itr5)
B_0x10002:Internal Trigger 6 (tim_itr6)
B_0x10003:Internal Trigger 7 (tim_itr7)
B_0x10004:Internal Trigger 8 (tim_itr8)
B_0x10005:Internal Trigger 9 (tim_itr9)
B_0x10006:Internal Trigger 10 (tim_itr10)
B_0x10007: Internal trigger 11 (tim_itr11)
B_0x20000: Internal trigger 12 (tim_itr12)
B_0x20001: Internal trigger 13 (tim_itr13)
B_0x20002: Internal trigger 14 (tim_itr14)
B_0x20003: Internal trigger 15 (tim_itr15)

(and repeat that pattern for all other fields that are splitted acrose registers)

Then one can code by just shifting the chosen enum to the TS1 field position.

This topic has been closed for replies.

2 replies

ST Technical Moderator
Nov 27, 2024 3:33 PM UTC

Hello @hijax_pl,

I have forwarded this request internally to the relevant team via Internal ticket number: 197197 (this tracking number is only for ST reference, and not accessible or usable by customers).

Thank you again for your contribution.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Dec 23, 2024 12:40 PM UTC

Hello @hijax_pl,

The svd files has been updated and I attached the STM32H5 svd package here.

Note that for the "TS" field declared in two positions, we can't implement all of the enumeration values, which causes the appearance of a warning in this case.

To align with validation tools, we implemented this:

  • TS[6:4] The enumeration values stop at "00111: External Trigger input (tim_etrf)".
  • TS[21:20] The enumeration values stop at "00011: Internal Trigger 3 (tim_itr3)".

and the same for SMS filed :

  • SMS[3:0] the enumerated values stop at "0111: External Clock mode 1 - Rising edges of the selected trigger (tim_trgi) clock the counter."
  • SMS[16]: the enumerated values stop at "0001: Quadrature encoder mode 1, x2 mode- Counter counts up/down on tim_ti1fp1 edge depending on tim_ti2fp2 level.".

 

Thank you again for the continued feedback; it is much appreciated!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks