Skip to main content
hijax_pl
Associate III
Nov 23, 2024 3:05 PM UTC
Question

SVD errors on STM32H503

Using python I have written small app to convert SVD V1.4 into assembly include. Then I started to write assemby code using RM0492 Rev2 .

For the peripherals I use (RCC,ADC,GPIO,GPDMA,TIM,USART) I have found that there are few errors in the SVD file, some typos etc.

Namely:

RCC_CCIPR5 register has only 2 fields described, no info about FDCANSEL, DACSEL & ADCDACSEL

RCC_CFGR regsiter shall be named RCC_CFGR1

For RCC_PLL1CFGR & RCC_PLL2CFGR there are DIVMx while should be PLLxM

 

 

 

This topic has been closed for replies.

4 replies

STTwo-32
ST Technical Moderator
Nov 23, 2024 4:44 PM UTC

Hello @hijax_pl 

Thank you for reporting those typos. I'm escalating the second and the third points as they are for correction (under internal ticket number 197881). But the first point, I find that we have a typo only on the name and description of the bit values for DACSEL. They others looks fine on my side.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
hijax_pl
hijax_plAuthor
Associate III
Nov 23, 2024 6:26 PM UTC

Yes, my mistake.

I have filtered out DAC & FDCAN as peripherals but also from RCC defines.

And yes, DACSEL is DAC1SEL in reference manual.

 

 

hijax_pl
hijax_plAuthor
Associate III
Nov 24, 2024 7:06 PM UTC

Do not know if I shall open new thread but anyway.

(1) Why TIM1_SMCR and TIM2/3_SMCR have different naming convetions for SMS / TS fields?

i.e. for TIM1_SMCR there are SMS/SMS_1 and TS/TS_1 and for TIM2/3_SMCR, SMS1/SMS2 and TS1/TS2 respectively.

(2) Also TIM1_SMCR_TS_1 field has no enumerated values, while for TIM2/3_SMCR_TS2 there are, but wrongly described. TIM1_SMCR_TS & TIM2/3_SMCR_TS1 has enums for the range 0..7 only, ie. the TS1 field itself.

As in the RM those fields must be combined, I think the easies way forward would be to provide enums only for the TS1 field, and add missing values:

B_0x10000:Internal Trigger 4 (tim_itr4)
B_0x10001:Internal Trigger 5 (tim_itr5)
B_0x10002:Internal Trigger 6 (tim_itr6)
B_0x10003:Internal Trigger 7 (tim_itr7)
B_0x10004:Internal Trigger 8 (tim_itr8)
B_0x10005:Internal Trigger 9 (tim_itr9)
B_0x10006:Internal Trigger 10 (tim_itr10)
B_0x10007: Internal trigger 11 (tim_itr11)
B_0x20000: Internal trigger 12 (tim_itr12)
B_0x20001: Internal trigger 13 (tim_itr13)
B_0x20002: Internal trigger 14 (tim_itr14)
B_0x20003: Internal trigger 15 (tim_itr15)

(and repeat that pattern for all other fields that are splitted acrose registers)

Then one can code by just shifting the chosen enum to the TS1 field position.