Skip to main content
neutroncode
Associate
Dec 2, 2025 8:06 PM UTC
Solved

SuperTinyKernel (STK) - lightweight embedded multi/single-core multithreading

Hi STM Devs!

I would like to introduce a thread scheduling library - SuperTinyKernel (STK).

Its GitHub repo: https://github.com/dmitrykos/stk

You can check capabilities in detail on GitHub but briefly STK can:

  • Soft and hard real-time support: STK supports cooperative scheduling for “soft real-time” tasks, you can also enable hard real-time mode (KERNEL_HRT) for periodic tasks with guaranteed deadlines.
  • Static and dynamic tasks: Define all tasks at startup (KERNEL_STATIC) or allow tasks to be created and destroyed at runtime (KERNEL_DYNAMIC).
  • Low-power friendliness: STK puts MCU into a low-power mode when there are no runnable tasks (task calls Sleep).
  • Tiny footprint: Minimal C++ abstractions (no STL, no heavy namespaces) keep the kernel small and simple.
  • Portability: Supports ARM Cortex-M and RISC-V RV32 MCUs.
  • Multi-core support: Fully implemented for Cortex-M and RISC-V.
  • x86 development mode: Compile & debug your code on a PC before flashing to the MCU, which helps with early testing and unit tests.
  • Open-source License: MIT: Open for commercial, closed-source, open-source - your choice.

There are ready to use STM32 examples for STM32F051 MCU (STM32F0DISCOVERY dev board), STM32F103 (NUCLEO-F103RB dev board), STM32F407 (STM32F4DISCOVERY dev board): 

https://github.com/dmitrykos/stk/tree/main/build/example/project/eclipse/stm

Any questions? Please ask, also you are welcome to participate in STK's GitHub repository.

Issamos
IssamosBest answer
Super User
Dec 2, 2025 8:13 PM UTC

Hello @neutroncode 

Thank you so much for sharing this repo with the community. Hope that ST Create a dedicated space for user’s contribution on the ST Community. This will help users to find helpful examples or inspiration for new projects.

Best Regards.

II

3 replies

Issamos
IssamosBest answer
Super User
Dec 2, 2025 8:13 PM UTC

Hello @neutroncode 

Thank you so much for sharing this repo with the community. Hope that ST Create a dedicated space for user’s contribution on the ST Community. This will help users to find helpful examples or inspiration for new projects.

Best Regards.

II

neutroncode
Associate
Dec 3, 2025 1:22 PM UTC

Hi @Issamos

Thank you for a warm welcome! 

STK is probably one of the easiest and fastest ways to add multi-threading to STM32 MCUs for new and existing bare-metal ISR-only projects, it has no board-specific dependencies or portability layers, fits any custom design based on STM32 MCU. Therefore I hope ST Community will find it useful and practical.

Best regards,

Dmitry.

neutroncode
Associate
Jan 29, 2026 4:48 PM UTC

Since the initial post there was an active development happening on STK and it has grown to a more convenient tool for embedded development, so wanted to highlight the progress:

  • Scheduling strategies: Besides existing Round-Robin (RR) new scheduling strategies were added: Fixed-Priority (FP, similar to FreeRTOS), Smooth Weighted Round-Robin (SWRR), Rate-Monotonic (RM), Deadline-Monotonic (DM), including Worst Case Reaction Time (WCRT) analysis, Earliest Deadline First (EDF), custom (via ITaskSwitchStrategy). It is probably the only open-source scheduler that has such a rich set of scheduling strategies.

  • Synchronization API: Besides CriticalSection there is a set of synchronization primitives now: SpinLock, Mutex, Event, ConditionVariable, Semaphore, Pipe primitives for inter-task, inter-core synchronization. Synchronization is optional via KERNEL_SYNC kernel mode, so it does not bloat FLASH/RAM.

  • Traceability: STK now supports tracing of tasks scheduling with a SEGGER SystemView.

  • C interface: For C-only projects STK got a fully-featured C interface.

If there are any questions, please ask!