Skip to main content
DS.4
Senior
Jan 22, 2024 4:07 PM UTC
Question

Stuck in RTC_EnterInitMode

After connecting to a X-NUCLEO-LPM01A board for power consumption test , RTC init will not end.

Stuck in this while loop:

 

 tickstart = HAL_GetTick();
 /* Wait till RTC is in INIT state and if Time out is reached exit */
 while ((hrtc->Instance->ISR & RTC_ISR_INITF) == 0U)
 {
 if ((HAL_GetTick() - tickstart) > RTC_TIMEOUT_VALUE)
 {
 return HAL_TIMEOUT;
 }
 }

 

 Current solution: I have to program some example using stm32wbIDE, only that fixes it and I can now use my FW.

 

 

This topic has been closed for replies.

6 replies

ST Employee
Jan 23, 2024 2:15 PM UTC

Hello @DS.4 ,

Make sure the RTC APB clock is enabled by checking the RTCAPBEN bit field , this could be due to some missing steps in the configuration of RTC and its clock source . This is just a guess if this does not resolve your issue i need further details on your configuration to help you solve this problem.

BR 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DS.4
DS.4Author
Senior
Jan 23, 2024 2:18 PM UTC

I will check that, 

Weird thing is even after aligning my init process to that of the example, it still won't work.

I still have to program the example and later my code.

Visitor II
Jan 1, 2025 9:40 AM UTC

I am running into this same issue on an example project for the STM32WLE wireless MCU. Has a solution been found? Can I provide any information to help solve the problem?