Skip to main content
Associate
Jun 3, 2025 9:31 PM UTC
Question

Strange operation of Nx_WebServer example on STM32H735G-DK board

I am experimenting with the function of reading a file by receiving a user command in the Nx_WebServer example of STM32H735G-DK. 
When connecting Stlink, input the t key in the Com port (115200 bps) that appears and press Enter to read the dashboard.html file. 
After performing this function, a fault occurs in tx_event_flags_get(&finish_flag, 0x01, TX_AND_CLEAR, &actual_flags, TX_WAIT_FOREVER); of console.c that is executed. 
This event flag is for communication between the UART receive interrupt and console_thread, and it works normally if filex io is not performed. 
Please help me figure out why this problem occurs after calling the filex API.
This topic has been closed for replies.

1 reply

Associate
Jun 5, 2025 3:03 AM UTC

Hello

after increasing stack size of console thread into 4K,  the problem disappeared.

Thanks