Skip to main content
mzenn.280
Associate II
Oct 11, 2023 9:15 AM UTC
Question

strange long eth transmission

I am using  STM32H735AGI with freertos + lwip + no dcache

I have an udp echo server on the device and a udp echo client in python that runs on the pc

The client sends messages with a length of 3 TCP_MSS

In the following logs the first number is the tick count (milliseconds)

ETH_IRQ is printed just before HAL_ETH_IRQHandler, that calls HAL_ETH_RxCpltCallback, that osSignalSet a task

EVN_IRQ_RX is printed by the task: it calls HAL_ETH_ReadData and print pbuf->tot_len, then it calls netif.input

When lwip collects the fragments, it passes the message to the echo server, that prints "[udp] ricevo ..."

The server echoes back the message, and netif.linkoutput prints "TX pbuf->tot_len" and transmits with HAL_ETH_Transmit followed by HAL_ETH_ReleaseTxPacket 

I am expecting 1500B/100Mbit=.15ms

The first transactions are "good":

0000036512) DBG - ETH_IRQ             
0000036512) DBG - EVN_IRQ_RX
0000036512) DBG - 1514
0000036512) DBG - ETH_IRQ
0000036512) DBG - EVN_IRQ_RX
0000036512) DBG - 1514
0000036512) DBG - ETH_IRQ
0000036512) DBG - EVN_IRQ_RX
0000036512) DBG - 1462
0000036513) DBG - [udp] ricevo 4380 B da 10.1.20.254:F985
0000036513) DBG - TX 1514
0000036513) DBG - TX 1514
0000036513) DBG - TX 1462

In the same millisecond, 36512, 3 irq are managed and in the next ms the message is echoed back

I send a set of 100 messages and then collect the logs: after some sets I get

0000689520) DBG - ETH_IRQ
0000689520) DBG - EVN_IRQ_RX
0000689520) DBG - 1514
0000689520) DBG - ETH_IRQ
0000689520) DBG - EVN_IRQ_RX
0000689520) DBG - 1514
0000689520) DBG - ETH_IRQ
0000689520) DBG - EVN_IRQ_RX
0000689520) DBG - 1462
0000689521) DBG - [udp] ricevo 4380 B da 10.1.20.254:CFE4
0000689521) DBG - TX 1514
0000689522) DBG - TX 1514
0000689522) DBG - TX 1462

The reception works as before but now there is one more ms when transmitting

What is the cause of this behaviour? What can I do?

 

This topic has been closed for replies.

1 reply

Joe WILLIAMS
ST Employee
Nov 7, 2023 10:03 PM UTC

Hi mzenn.280

 

Your case is being reviewed via our ST Online Support System. 

 

Kind Regards

Joe WILLIAMS

STMicro Support