Skip to main content
Associate
Sep 3, 2024 8:16 PM UTC
Question

STMWB05xZ Enable CTE

Hi,

I am working on a project which will require a connectionless CTE to be added to the advertisement. From what I understand, there are not currently any examples of a configured CTE beacon. What would be the best example project to modify to create a connectionless CTE beacon? Are there any examples anywhere floating around that I am unaware of? Or could someone point me in the right dire

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
Sep 4, 2024 12:16 PM UTC

Hello @atrujillo 

STM32WB05 devices support standard Bluetooth LE Direction Finding Features and, as consequence, both connection and connection less mode.
Youl could refer to the related Bluetooth LE stack v4.x programming manual available on ST web site:https://www.st.com/resource/en/programming_manual/pm0274-bluetooth-low-energy-stack-v4x-programming-guidelines-stmicroelectronics.pdf
Section 2.11 Direction finding

Associated commands and events are documented on related Application Note: https://www.st.com/resource/en/application_note/an6142-introduction-to-stm32wb0-bluetooth-low-energy-wireless-interface-stmicroelectronics.pdf

Best regards

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
atrujilloAuthor
Associate
Sep 5, 2024 10:07 PM UTC

I have some code here for configuring a beacon. However, it doesn't seem to correctly configure the CTE. The functions all return BLE_STATUS_SUCCESS, but when sniffing the packets using wireshark, they do not seem to have a CTE attached. They do look like extended periodic advertising packets, but I do not see a CTE.

 

 Advertising_Set_Parameters_t Advertising_Set_Parameters;
 tBleStatus ret = BLE_STATUS_SUCCESS;

 uint8_t b_index = 0;
 extended_beacon[b_index] = 0x02;
 extended_beacon[++b_index] = AD_TYPE_FLAGS;
 extended_beacon[++b_index] = FLAG_BIT_LE_GENERAL_DISCOVERABLE_MODE | FLAG_BIT_BR_EDR_NOT_SUPPORTED;
 extended_beacon[++b_index] = strlen(ext_beacon_name) + 1;
 extended_beacon[++b_index] = AD_TYPE_COMPLETE_LOCAL_NAME;

 memcpy(&extended_beacon[++b_index], &ext_beacon_name, strlen(ext_beacon_name));
 b_index += strlen(ext_beacon_name);

 uint8_t m_data_len = 19;

 extended_beacon[++b_index] = m_data_len;
 extended_beacon[++b_index] = AD_TYPE_MANUFACTURER_SPECIFIC_DATA;
 --m_data_len;
 extended_beacon[++b_index] = 0x30;
 --m_data_len;
 extended_beacon[++b_index] = 0x00;
 --m_data_len;
 // set some extra data
 for (uint8_t i = 0; i < m_data_len; ++i)
 {
 extended_beacon[++b_index] = i;
 }

 extended_beacon[++b_index] = 0x02;
 extended_beacon[++b_index] = AD_TYPE_TX_POWER_LEVEL;
 extended_beacon[++b_index] = 0x18;


 Advertising_Set_Parameters.Advertising_Handle = 0;
 Advertising_Set_Parameters.Duration = 0;
 Advertising_Set_Parameters.Max_Extended_Advertising_Events = 0;

 // set advertising parameters
 ret = aci_gap_set_advertising_configuration(Advertising_Set_Parameters.Advertising_Handle,
 GAP_MODE_GENERAL_DISCOVERABLE,
 (HCI_ADV_EVENT_PROP_TXPOWER_INC),
 2056,
 2056,
 HCI_ADV_CH_ALL,
 HCI_ADDR_PUBLIC, /* ignored param */
 peeraddr, /* No peer address */
 HCI_ADV_FILTER_NONE,
 0, /* 0 dBm */
 HCI_PHY_LE_1M, /* Primary advertising PHY */
 0, /* 0 skips */
 HCI_PHY_LE_1M, /* Secondary advertising PHY. Not used with legacy advertising. */
 1, /* SID */
 0x00 /* No scan request notifications */);
 check_ble_success(ret, "aci_gap_set_advertising_configuration");

 // set advertising data
 ret = aci_gap_set_advertising_data(Advertising_Set_Parameters.Advertising_Handle, ADV_COMPLETE_DATA, sizeof(extended_beacon), extended_beacon);
 check_ble_success(ret, "aci_gap_set_advertising_data");

 ret = GAP_set_extended_advertising_data(Advertising_Set_Parameters.Advertising_Handle, ADV_COMPLETE_DATA, sizeof(extended_beacon), extended_beacon);
 check_ble_success(ret, "GAP_set_extended_advertising_data");

 // set periodic advertisement parameters
 ret = hci_le_set_periodic_advertising_parameters(Advertising_Set_Parameters.Advertising_Handle,
 1000,
 2056,
 0x0040);
 check_ble_success(ret, "hci_le_set_periodic_advertising_parameters");

 // set connectionless cte parameters
 ret = hci_le_set_connectionless_cte_transmit_parameters(Advertising_Set_Parameters.Advertising_Handle,
 0x14, // length (0x02...x014)
 CTE_AOA, //type (AoA tone extension)
 0x01, // count
 0x00, // antenna count
 NULL /*antenna array*/);
 check_ble_success(ret, "hci_le_set_connectionless_cte_transmit_parameters");

 // enable periodic advertisement
 ret = hci_le_set_periodic_advertising_enable(0x02, Advertising_Set_Parameters.Advertising_Handle);
 check_ble_success(ret, "hci_le_set_periodic_advertising_enable");

 // set connectionless cte transmit enable
 ret = hci_le_set_connectionless_cte_transmit_enable(Advertising_Set_Parameters.Advertising_Handle ,1);
 check_ble_success(ret, "hci_le_set_connectionless_cte_transmit_enable");

 // enable advertising
 ret = aci_gap_set_advertising_enable(1, 1, &Advertising_Set_Parameters);
 check_ble_success(ret, "aci_gap_set_advertising_enable");