Skip to main content
Associate III
March 28, 2026
Solved

[stm32u585] wakeup failed from standby mode, "Wait till LSI is disabled" timeout in HAL_RCC_OscConfig()

hello,

I encountered a problem while developing for stm32u585. When the stm32 wakes up from standby mode, the HAL_RCC_OscConfig() function occasionally fails, "Wait till LSI is disabled" timeout in HAL_RCC_OscConfig() (this project uses IWDG)
The specific process is as follows:

1. start boot
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 MX_ICACHE_Init();
 MX_UART4_Init();
 boot to other address(app)
2. app init
 HAL_Init();
 SystemClock_Config();
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSI
 |RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON_RTC_ONLY;
 RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON;
 RCC_OscInitStruct.LSIDiv = RCC_LSI_DIV128;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 40;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
3. timeout in HAL_RCC_OscConfig()
 /* Turn off LSI before changing RCC_BDCR_LSIPREDIV */
 if ((bdcr_temp & RCC_BDCR_LSION) == RCC_BDCR_LSION)
 {
 __HAL_RCC_LSI_DISABLE();

 tickstart = HAL_GetTick();

 /* Wait till LSI is disabled */
 while (READ_BIT(RCC->BDCR, RCC_BDCR_LSIRDY) != 0U)
 {
 if ((HAL_GetTick() - tickstart) > LSI_TIMEOUT_VALUE)
 {
 return HAL_TIMEOUT;
 }
 }
 }

How to solve this problem

 

Saket_OmBest answer
ST Technical Moderator
March 30, 2026

Hello @lll 

The LSI should only be initialized once at power-on reset (POR). Re-initializing or reconfiguring the LSI after each wake-up from standby can cause issues, as the oscillator may already be in use by IWDG, and the LSIRDY flag may not behave as expected.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

5 replies

Saket_OmBest answer
ST Technical Moderator
March 30, 2026

Hello @lll 

The LSI should only be initialized once at power-on reset (POR). Re-initializing or reconfiguring the LSI after each wake-up from standby can cause issues, as the oscillator may already be in use by IWDG, and the LSIRDY flag may not behave as expected.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
lllAuthor
Associate III
March 30, 2026

Does this mean I have to modify HAL_RCC_OscConfig() ?

I have added this condition in HAL_RCC_OscConfig():

__HAL_PWR_GET_FLAG(PWR_FLAG_SBF)

Can it ensure that this startup is from standby wake-up

/*------------------------------ LSI Configuration -------------------------*/
 if ((((pRCC_OscInitStruct->OscillatorType) & RCC_OSCILLATORTYPE_LSI) == RCC_OSCILLATORTYPE_LSI)
 && __HAL_PWR_GET_FLAG(PWR_FLAG_SBF))