Skip to main content
Associate III
Sep 3, 2024 7:08 AM UTC
Solved

stm32u585 ux_device_hid example without USBPD

I can open, regenerate, build and flash B-U585I-IOT02A -> Ux_Device_HID example successfully. 
But when I try disable USBPD (we don't have usbpd on our board. just the D+ and D- pins) and regenerate the project, so many many unrelated files are being removed or added from the project and it becomes very hard to compile it and use it. 
Is there any example for stm32u585 without USBPD?

This topic has been closed for replies.

6 replies

ST Technical Moderator
Sep 3, 2024 12:20 PM UTC

 


@miladmohtashamirad wrote:


But when I try disable USBPD (we don't have usbpd on our board. just the D+ and D- pins) 


Hi @miladmohtashamirad 

Do you mean without Type C connector? You can check examples provided stm32u5-classic-coremw-apps/Projects/NUCLEO-U575ZI-Q/Applications/USB_Device/HID_Standalone at main · STMicroelectronics/stm32u5-classic-coremw-apps (github.com)

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate III
Sep 3, 2024 11:19 PM UTC

Hi @FBL .
yes. I'm trying to get usb working on type C connector without USBPD. 
This project is also using USBPD. ( I might be wrong, but in the main loop and in the source code I can see USBPD stuff).
Thanks. 

 

Explorer
Sep 3, 2024 12:33 PM UTC

hi @miladmohtashamirad 

 

Can you first share with us the .ioc of your project ? 

Associate III
Sep 3, 2024 11:18 PM UTC

Hi @Mohamed_AYED .
The ioc file is exactly as the original B-U585I-IOT02A -> Ux_Device_HID example. only USBPD in connectivity and middleware and it's dma channels are disabled and then regenerated. I've attached the project here.
One of the odd things to see is USBX\App\ux_device_descriptors.c that is malformed. 

Associate III
Sep 4, 2024 12:07 AM UTC

Hi @Mohamed_AYED ,
I think I found what the problem was. I needed to revert some changes. 
Kind Regards.

Mohamed_AYEDBest answer
Explorer
Sep 3, 2024 11:43 PM UTC