Skip to main content
Associate III
Jan 29, 2026 3:42 PM UTC
Solved

[stm32u585] program is stuck in HAL_UART_IRQHandler with TC flag

hello

Description:

I'm currently working with the STM32U585 and encountered an issue related to USART3

Most of the time the code works fine, but it occasionally gets trapped in HAL_UART_IRQHandler

I am using the DMA Receiver Timeout (RTO) and DMA TX, may code is:

void uart_tx_complete_cb(UART_HandleTypeDef *huart)
{
 if (...)
 HAL_UART_Transmit_DMA(huart, buf, len);
}
void uart_rx_error_cb(UART_HandleTypeDef *huart)
{
 HAL_UART_AbortReceive(huart);
 if (huart->ErrorCode & HAL_UART_ERROR_RTO)
 {
 ...
 }
 HAL_UART_Receive_DMA(huart, rx_buf, rx_buf_len);
}
HAL_UART_RegisterCallback(&huart3, HAL_UART_ERROR_CB_ID, uart_rx_error_cb);
HAL_UART_ReceiverTimeout_Config(&huart3, 100);
HAL_UART_EnableReceiverTimeout(&huart3);
HAL_UART_Receive_DMA(&TD_UART_HANDLE, rx_buf, rx_buf_len);
HAL_UART_RegisterCallback(&huart3, HAL_UART_TX_COMPLETE_CB_ID, uart_tx_complete_cb);

 

When the issue occurs, I found that the TC (Transmission Complete) flag is not being cleared:

1.PNG2.PNG

and HAL_UART_IRQHandler return at /* End if some error occurs */

lllBest answer
Associate III
Feb 9, 2026 8:25 AM UTC

thank you all

@Ozone @Saket_Om @TDK 

I move HAL_UART_Transmit_DMA() out of uart_tx_complete_cb()

and use HAL_UARTEx_ReceiveToIdle_DMA() instead of HAL_UART_EnableReceiverTimeout()

to circumvent this issue, it seems to be working well

6 replies

ST Technical Moderator
Jan 29, 2026 3:59 PM UTC

Hello @lll 

Did you investigate why it is not clearing the TC flag inside HAL_UART_IRQHandler?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
TDK
Jan 30, 2026 12:14 AM UTC

You restart the transfer on every tx complete, so TC flag will continue to get set. What makes you think it is stuck? Stepping through should let you see the logic where it gets cleared. TC flag doesn’t necessarily even need to be cleared.

If it “works most of the time”, problem is likely not with the logic inside the handler.

"If you feel a post has answered your question, please click ""Accept as Solution""."
lllAuthor
Associate III
Jan 30, 2026 3:56 AM UTC

TC and TCIE are both set, and HAL_UART_IRQHandler returned before:

/* UART in mode Transmitter (transmission end) -----------------------------*/

UART_EndTransmit_IT

 

After problem occurs, any suspension will stop at HAL_UART_IRQHandler, I set a breakpoint in uart_tx_complete_cb, and never go in it

ST Technical Moderator
Feb 3, 2026 9:53 AM UTC

Hello @lll 

Could you please share a minimal example to reproduce the issue ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Ozone
Principal
Feb 3, 2026 10:03 AM UTC

I think you can look up yourself  which operations clear the TC flag.

However, consider your callback routine takes too long,and flag is already set again when it exists.
In this case, you need to move processing code out of the interrupt context.

lllAuthorBest answer
Associate III
Feb 9, 2026 8:25 AM UTC

thank you all

@Ozone @Saket_Om @TDK 

I move HAL_UART_Transmit_DMA() out of uart_tx_complete_cb()

and use HAL_UARTEx_ReceiveToIdle_DMA() instead of HAL_UART_EnableReceiverTimeout()

to circumvent this issue, it seems to be working well