Skip to main content
Associate
September 10, 2026
Solved

STM32U575CGU3: Does ADC_Init leave analog bias active? Looking for others who observed similar current increase

  • September 10, 2026
  • 2 replies
  • 53 views

Hi,

On STM32U575CGU3, I see a reproducible +200 µA increase in current after calling MX_ADC1_Init() once. Even after HAL_ADC_DeInit(), ADC reset, and disabling VddA, the additional current does not return to the original baseline.

Here is the minimal code:

c

int main(void)
{
HAL_Init();
SystemClock_Config();

MX_GPIO_Init();
MX_GPDMA1_Init();
MX_ADC1_Init(); // +200uA increase
MX_OCTOSPI1_Init();
MX_SPI1_Init();
MX_USB_OTG_FS_PCD_Init();
MX_USART1_UART_Init();
MX_ICACHE_Init();

// ADC Disable
HAL_ADC_DeInit(&hadc1);
__HAL_RCC_ADC1_FORCE_RESET();
__HAL_RCC_ADC1_RELEASE_RESET();
HAL_PWREx_DisableVddA();

while (1) {
__NOP();
}
}

Questions

  • Has anyone observed similar behavior on U5 devices (ADC bias or VREFBUF staying active after initialization)?

  • Are there known conditions where ADC/VREFBUF analog blocks remain powered even after DeInit and VddA OFF?

  • Any hints on additional steps required to fully shut down the analog domain?

Thanks.

Best answer by KDJEM.1

Hello ​@k.morohoshi ;

 

 Can you check and share which ADC kernel clock source STM32CubeMX generated for ADC on your project?

I recommend you to use HCLK clock source.

 

Thank you.

Kaouthar

2 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
September 23, 2026

Hello ​@k.morohoshi ;

 

 Can you check and share which ADC kernel clock source STM32CubeMX generated for ADC on your project?

I recommend you to use HCLK clock source.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Associate
September 29, 2026

Thank you for the suggestion. I checked the ADC kernel clock source generated by STM32CubeMX, and it was originally set to HSI. After changing the ADC kernel clock to HCLK as recommended, the additional current (~200 µA) disappeared.

So the issue was caused by the ADC kernel clock selection. With HCLK as the kernel clock, the analog domain shuts down correctly and the current returns to the expected baseline.

Additional observation: Before switching to HCLK, calling HAL_ADC_DeInit(), forcing ADC reset, and disabling VddA did not reduce the current. It seems that once MX_ADC1_Init() is executed, some analog bias remains active in RUN mode when the ADC kernel clock is HSI. After switching to HCLK, STOP2 also works correctly and the current drops to the expected low‑power level.

This may help others who observe similar behavior on U5 devices.

Thanks again for the support.