Skip to main content
Associate
Sep 9, 2026 2:02 AM UTC
Question

STM32U575CGU3: ADC_Init enables analog bias that cannot be disabled by ADC_DeInit?

Hi,

On STM32U575CGU3, calling MX_ADC1_Init() once increases the device current by about +200 µA. After that, even if I run HAL_ADC_DeInit(), reset ADC1, and disable VddA, the extra +200 µA current does not disappear.

Here is the minimal code:

c

int main(void)
{
HAL_Init();
SystemClock_Config();

MX_GPIO_Init();
MX_GPDMA1_Init();
MX_ADC1_Init(); // <-- Base +200uA increase
MX_OCTOSPI1_Init();
MX_SPI1_Init();
MX_USB_OTG_FS_PCD_Init();
MX_USART1_UART_Init();
MX_ICACHE_Init();

// ADC Disable
HAL_ADC_DeInit(&hadc1); // <-- This does NOT reduce the +200uA
__HAL_RCC_ADC1_FORCE_RESET();
__HAL_RCC_ADC1_RELEASE_RESET();
HAL_PWREx_DisableVddA();

while (1) {
__NOP();
}
}

Question

Does ADC_Init enable an internal analog bias that cannot be fully disabled by ADC_DeInit, ADC reset, or VddA OFF? Is there any complete shutdown procedure to fully power down ADC/VREFBUF after initialization?

Thanks.

1 reply

ST Technical Moderator
Oct 22, 2026 10:10 AM UTC

Hello ​@k.morohoshi 

The issue you encounter seems to be related to the errata 2.9.2

Please try to apply one of the workarounds mentioned in the errata. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om