Skip to main content
Associate II
Jan 28, 2026 8:05 PM UTC
Question

STM32U575 Secure and non-secure function calls

Hi 

I have been testing secure function calls from non-secure world in STM32U575 - TrustZone Enabled environment.

I have a LED_Port which is in secure world (secure peripheral). I have implemented a toggle function in secure project - secure_nsc.c/h

CMSE_NS_ENTRY void SECURE_BlinkBlueLED(void) {...}

I can be able to compile without any issues:

Here are some linker details:

Suthan_0-1769630214952.png

.....................................

Suthan_1-1769630234076.png

I verified the map files as below

Suthan_2-1769630280746.png

.......................

Suthan_3-1769630311904.png

Now I am calling this function from non-secure project: It went to Hard Fault as it calls original function which is in the secure world.

Suthan_4-1769630516386.png

How to call veneer instead of direct function?

Any help?

 

 

 

1 reply

ST Technical Moderator
Jan 29, 2026 9:37 AM UTC

Hello @Suthan 

On STM32U5 with TrustZone, the non‑secure code must never call the secure implementation directly; instead, it has to call the veneer located in the NSC (Non‑Secure Callable) region. To achieve this, the function must be declared with `CMSE_NS_ENTRY` in a source file that is linked into the NSC region (for example `secure_nsc.c`), and the non‑secure project must include the corresponding NSC header (for example `secure_nsc.h`) and call that symbol. Please verify that `secure_nsc.o` is placed in the NSC section in the secure linker script and that in your non‑secure map file the symbol `SECURE_BlinkBlueLED` points to an address in the NSC region; otherwise the non‑secure code will attempt to jump directly into secure flash and trigger a HardFault.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om