Skip to main content
Associate II
July 5, 2026
Solved

[STM32U575][GPDMA] Linked-list node fetch fails when a 36-byte node crosses 64KB SRAM1 boundaries (0x20010000, 0x20020000)

Hello:
Observation (empirical, multiple boundaries confirmed):

When placing DMA linked list nodes (36 bytes each = 9 words) sequentially in SRAM1,

if a single node spans certain addresses, the GPDMA channel enters DTEF state

when fetching that node.

 

Confirmed problematic boundaries in SRAM1 (192KB, 0x20000000 - 0x2002FFFF):

- 0x20010000 : crossing FAILS

- 0x20020000 : crossing FAILS

 

Both boundaries appear at 64KB intervals within SRAM1, which suggests

that SRAM1 may be internally organized as multiple 64KB blocks/banks.

 

Test cases:

Test 1: Node array starting at 0x20011A54 (natural placement)

- Nodes 1-1633: within bank containing 0x20010000-0x2001FFFF → OK

- Node 1634: spans 0x2001FFF8 - 0x2002001C → FAILS (crosses 0x20020000)

 

Test 2: Node array starting at (0x20010000 - 44)

- The first node spans 0x2000FFD4 - 0x2000FFF8 (OK)

- The second node spans 0x2000FFF8 - 0x2001001C → FAILS (crosses 0x20010000)

 

Test 3: Node array starting at (0x20010000 - 36)

- The first node ends exactly at 0x20010000

- No node crosses the boundary → OK

 

Root cause (inferred):

GPDMA appears to fetch each 36-byte linked list node as a single burst,

and this burst cannot cross what appears to be a 64KB internal SRAM1

boundary.

 

Workaround:

Place the entire linked list node array within a single 64KB region

by using explicit address placement:

static DMA_NodeTypeDef g_dmaNodes[N] @ 0x20010000;

 

Questions to STMicro:

1. Is SRAM1 internally organized as multiple 64KB banks/blocks?

2. Is this crossing limitation of GPDMA documented anywhere?

3. Should HAL_DMAEx_List_BuildNode validate node placement?

4. Are there other similar boundaries elsewhere (SRAM2, SRAM3)?
5. If this behavior is not currently documented in ES0499, could it be considered for inclusion in a future revision of the errata sheet?

I have checked ES0499 (latest revision available on st.com as of July 2026) and could not find any documented entry describing this behavior. I have also reviewed related community threads (e.g., #141509 'GPDMA with linked list for big buffers') which mention the 64KB limitation but do not specifically address linked-list node fetch crossing internal SRAM1 boundaries.

Khaled_DHIFBest answer
ST Employee
July 9, 2026

Hello ​@mikesmith100 ,

This is actually mentioned in the RM0456 for the STM32U575, in the GPDMA_CxLLR description (page 762).

The manual says the entire linked-list data structure must stay within the 64-Kbyte space defined by GPDMA_CxLBAR. So, if a node crosses that boundary, the GPDMA can fail with DTEF.

So, it looks like this is a known GPDMA linked-list limitation, not really a SRAM1 issue.

Best,

DHIF Khaled

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"

1 reply

Khaled_DHIFBest answer
ST Employee
July 9, 2026

Hello ​@mikesmith100 ,

This is actually mentioned in the RM0456 for the STM32U575, in the GPDMA_CxLLR description (page 762).

The manual says the entire linked-list data structure must stay within the 64-Kbyte space defined by GPDMA_CxLBAR. So, if a node crosses that boundary, the GPDMA can fail with DTEF.

So, it looks like this is a known GPDMA linked-list limitation, not really a SRAM1 issue.

Best,

DHIF Khaled

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"