Skip to main content
Associate II
July 16, 2026
Solved

STM32U575 freezes when exiting STOP2 mode after power cycle

The MCU works fine the first time it gets programmed. However, after one power cycle, it freezes completely after an external  interrupt happens. Doesn’t even enter the error handler. I have SMPS enabled. Thanks for your help

 

int main(void)
{

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

/* MCU Configuration--------------------------------------------------------*/

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();

/* USER CODE BEGIN Init */

/* USER CODE END Init */

/* Configure the System Power */
SystemPower_Config();

/* Configure the system clock */
SystemClock_Config();

/* USER CODE BEGIN SysInit */

/* USER CODE END SysInit */

/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_RTC_Init();
MX_UART4_Init();
/* USER CODE BEGIN 2 */
GreenLEDOn();
HAL_Delay(5000);
GreenLEDOff();
/* USER CODE END 2 */

/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
if(!HAL_GPIO_ReadPin(V_Fu_Trig_GPIO_Port, V_Fu_Trig_Pin))//Fuse voltage fault
{
fault = true;
Enter_Stop2_Mode();
NVIC_SystemReset();
}
else
flashRedLED();

HAL_Delay(2000);


/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}


static void Enter_Stop2_Mode(void)
{

HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_SLEEPENTRY_WFI);
}

 

yycBest answer
Associate II
September 25, 2026

Hello Gyessine,

 

Thank you for your followup. 

 

It turns out I need to put all of my declared variables and struct into SRAM4 by modifying the “STM32U575RITXQ_FLASH.ld” file. I noticed that the unit would get into a hard fault error state after waking up, then it turned out to be SRAM 1~3 were powered down in STOP2 mode. Only data in SRAM4 in retained by default.

 

Youyou

10 replies

Gyessine
ST Technical Moderator
July 17, 2026

Hello ​@yyc 
Are you using a custom PCB or a reference board.

Stop 2 mode was tested with this firmware example on an STM32 Nucleo- U575 board, and the issue could not be reproduced.

For now, use the firmware example.

If a reference board is used and the example works, the issue is likely related to the software implementation. The example can then be used as a reference.

If a custom printed circuit board (PCB) is used and the project still does not work with the firmware example, the issue might be related to hardware.
BR
Gyessine

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yycAuthor
Associate II
July 17, 2026

I am using a custom PCB, but the it works with the example.

It seems like the problem is related to my code. But I cannot tell if I’ve done anything wrong. I am using the default setup. I am attaching my whole file here. Thanks for your help.

/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2026 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdint.h>
#include <string.h>
#include <stdio.h>
#include <stdlib.h>
#include <ctype.h>
#include <stdbool.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define GreenLEDOn() (HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, SET))
#define GreenLEDOff() (HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, RESET))
#define RedLEDOn() (HAL_GPIO_WritePin(LED_R_GPIO_Port, LED_R_Pin, SET))
#define RedLEDOff() (HAL_GPIO_WritePin(LED_R_GPIO_Port, LED_R_Pin, RESET))
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc4;

COMP_HandleTypeDef hcomp1;

OPAMP_HandleTypeDef hopamp1;

RTC_HandleTypeDef hrtc;

UART_HandleTypeDef huart4;
DMA_HandleTypeDef handle_GPDMA1_Channel0;

/* USER CODE BEGIN PV */
bool fault = false;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void SystemPower_Config(void);
static void MX_GPIO_Init(void);
static void MX_GPDMA1_Init(void);
static void MX_ADC4_Init(void);
static void MX_COMP1_Init(void);
static void MX_RTC_Init(void);
static void MX_UART4_Init(void);
static void MX_OPAMP1_Init(void);
static void MX_ICACHE_Init(void);
/* USER CODE BEGIN PFP */
void flashGreenLED();
void flashRedLED();
static void Enter_Stop2_Mode();
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

/* MCU Configuration--------------------------------------------------------*/

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();

/* USER CODE BEGIN Init */

/* USER CODE END Init */

/* Configure the System Power */
SystemPower_Config();

/* Configure the system clock */
SystemClock_Config();

/* USER CODE BEGIN SysInit */

/* USER CODE END SysInit */

/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_GPDMA1_Init();
MX_ADC4_Init();
MX_COMP1_Init();
MX_RTC_Init();
MX_UART4_Init();
MX_OPAMP1_Init();
MX_ICACHE_Init();
/* USER CODE BEGIN 2 */
GreenLEDOn();
HAL_Delay(8000);
GreenLEDOff();
/* USER CODE END 2 */

/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
if(!HAL_GPIO_ReadPin(V_Fu_Trig_GPIO_Port, V_Fu_Trig_Pin))//Fuse voltage fault
{
fault = true;
Enter_Stop2_Mode();
NVIC_SystemReset();
}
else
flashRedLED();

HAL_Delay(2000);


/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}

/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE3) != HAL_OK)
{
Error_Handler();
}

/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI
|RCC_OSCILLATORTYPE_MSIK;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_4;
RCC_OscInitStruct.MSIKClockRange = RCC_MSIKRANGE_15;
RCC_OscInitStruct.MSIKState = RCC_MSIK_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 32;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 64;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_0;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}

/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}

/**
* @brief Power Configuration
* @retval None
*/
static void SystemPower_Config(void)
{

/*
* Disable the internal Pull-Up in Dead Battery pins of UCPD peripheral
*/
HAL_PWREx_DisableUCPDDeadBattery();

/*
* SRAM Power Down In Stop Mode Config
*/
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM1_PAGE1_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM1_PAGE2_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM1_PAGE3_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM2_PAGE1_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM2_PAGE2_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM3_PAGE1_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM3_PAGE2_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM3_PAGE3_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM3_PAGE4_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM3_PAGE5_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM3_PAGE6_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM3_PAGE7_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_SRAM3_PAGE8_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_DCACHE1_FULL_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_DMA2DRAM_FULL_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_PKA32RAM_FULL_STOP_RETENTION);
HAL_PWREx_DisableRAMsContentStopRetention(PWR_PERIPHRAM_FULL_STOP_RETENTION);

/*
* Switch to SMPS regulator instead of LDO
*/
if (HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN PWR */
/* USER CODE END PWR */
}

/**
* @brief ADC4 Initialization Function
* @param None
* @retval None
*/
static void MX_ADC4_Init(void)
{

/* USER CODE BEGIN ADC4_Init 0 */

/* USER CODE END ADC4_Init 0 */

ADC_ChannelConfTypeDef sConfig = {0};

/* USER CODE BEGIN ADC4_Init 1 */

/* USER CODE END ADC4_Init 1 */

/** Common config
*/
hadc4.Instance = ADC4;
hadc4.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc4.Init.Resolution = ADC_RESOLUTION_12B;
hadc4.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc4.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc4.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc4.Init.LowPowerAutoPowerOff = ADC_LOW_POWER_NONE;
hadc4.Init.LowPowerAutoWait = DISABLE;
hadc4.Init.ContinuousConvMode = DISABLE;
hadc4.Init.NbrOfConversion = 1;
hadc4.Init.DiscontinuousConvMode = DISABLE;
hadc4.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc4.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc4.Init.DMAContinuousRequests = DISABLE;
hadc4.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_LOW;
hadc4.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc4.Init.SamplingTimeCommon1 = ADC4_SAMPLETIME_1CYCLE_5;
hadc4.Init.SamplingTimeCommon2 = ADC4_SAMPLETIME_1CYCLE_5;
hadc4.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc4) != HAL_OK)
{
Error_Handler();
}

/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC4_RANK_CHANNEL_NUMBER;
sConfig.SamplingTime = ADC4_SAMPLINGTIME_COMMON_1;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC4_Init 2 */

/* USER CODE END ADC4_Init 2 */

}

/**
* @brief COMP1 Initialization Function
* @param None
* @retval None
*/
static void MX_COMP1_Init(void)
{

/* USER CODE BEGIN COMP1_Init 0 */

/* USER CODE END COMP1_Init 0 */

/* USER CODE BEGIN COMP1_Init 1 */

/* USER CODE END COMP1_Init 1 */
hcomp1.Instance = COMP1;
hcomp1.Init.InputPlus = COMP_INPUT_PLUS_IO2;
hcomp1.Init.InputMinus = COMP_INPUT_MINUS_IO1;
hcomp1.Init.OutputPol = COMP_OUTPUTPOL_NONINVERTED;
hcomp1.Init.WindowOutput = COMP_WINDOWOUTPUT_EACH_COMP;
hcomp1.Init.Hysteresis = COMP_HYSTERESIS_MEDIUM;
hcomp1.Init.BlankingSrce = COMP_BLANKINGSRC_NONE;
hcomp1.Init.Mode = COMP_POWERMODE_ULTRALOWPOWER;
hcomp1.Init.WindowMode = COMP_WINDOWMODE_DISABLE;
hcomp1.Init.TriggerMode = COMP_TRIGGERMODE_NONE;
if (HAL_COMP_Init(&hcomp1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN COMP1_Init 2 */

/* USER CODE END COMP1_Init 2 */

}

/**
* @brief GPDMA1 Initialization Function
* @param None
* @retval None
*/
static void MX_GPDMA1_Init(void)
{

/* USER CODE BEGIN GPDMA1_Init 0 */

/* USER CODE END GPDMA1_Init 0 */

/* Peripheral clock enable */
__HAL_RCC_GPDMA1_CLK_ENABLE();

/* GPDMA1 interrupt Init */
HAL_NVIC_SetPriority(GPDMA1_Channel0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(GPDMA1_Channel0_IRQn);

/* USER CODE BEGIN GPDMA1_Init 1 */

/* USER CODE END GPDMA1_Init 1 */
/* USER CODE BEGIN GPDMA1_Init 2 */

/* USER CODE END GPDMA1_Init 2 */

}

/**
* @brief ICACHE Initialization Function
* @param None
* @retval None
*/
static void MX_ICACHE_Init(void)
{

/* USER CODE BEGIN ICACHE_Init 0 */

/* USER CODE END ICACHE_Init 0 */

/* USER CODE BEGIN ICACHE_Init 1 */

/* USER CODE END ICACHE_Init 1 */

/** Enable instruction cache in 1-way (direct mapped cache)
*/
if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK)
{
Error_Handler();
}
if (HAL_ICACHE_Enable() != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ICACHE_Init 2 */

/* USER CODE END ICACHE_Init 2 */

}

/**
* @brief OPAMP1 Initialization Function
* @param None
* @retval None
*/
static void MX_OPAMP1_Init(void)
{

/* USER CODE BEGIN OPAMP1_Init 0 */

/* USER CODE END OPAMP1_Init 0 */

/* USER CODE BEGIN OPAMP1_Init 1 */

/* USER CODE END OPAMP1_Init 1 */
hopamp1.Instance = OPAMP1;
hopamp1.Init.PowerSupplyRange = OPAMP_POWERSUPPLY_HIGH;
hopamp1.Init.Mode = OPAMP_STANDALONE_MODE;
hopamp1.Init.NonInvertingInput = OPAMP_NONINVERTINGINPUT_IO0;
hopamp1.Init.InvertingInput = OPAMP_INVERTINGINPUT_IO0;
hopamp1.Init.PowerMode = OPAMP_POWERMODE_LOWPOWER_NORMALSPEED;
hopamp1.Init.UserTrimming = OPAMP_TRIMMING_FACTORY;
hopamp1.Init.TrimmingValueP = 16;
hopamp1.Init.TrimmingValueN = 16;
hopamp1.Init.TrimmingValuePLowPower = 16;
hopamp1.Init.TrimmingValueNLowPower = 16;
if (HAL_OPAMP_Init(&hopamp1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN OPAMP1_Init 2 */

/* USER CODE END OPAMP1_Init 2 */

}

/**
* @brief RTC Initialization Function
* @param None
* @retval None
*/
static void MX_RTC_Init(void)
{

/* USER CODE BEGIN RTC_Init 0 */

/* USER CODE END RTC_Init 0 */

RTC_PrivilegeStateTypeDef privilegeState = {0};
RTC_TimeTypeDef sTime = {0};
RTC_DateTypeDef sDate = {0};

/* USER CODE BEGIN RTC_Init 1 */

/* USER CODE END RTC_Init 1 */

/** Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
hrtc.Init.BinMode = RTC_BINARY_NONE;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}
privilegeState.rtcPrivilegeFull = RTC_PRIVILEGE_FULL_NO;
privilegeState.backupRegisterPrivZone = RTC_PRIVILEGE_BKUP_ZONE_NONE;
privilegeState.backupRegisterStartZone2 = RTC_BKP_DR0;
privilegeState.backupRegisterStartZone3 = RTC_BKP_DR0;
if (HAL_RTCEx_PrivilegeModeSet(&hrtc, &privilegeState) != HAL_OK)
{
Error_Handler();
}

/* USER CODE BEGIN Check_RTC_BKUP */

/* USER CODE END Check_RTC_BKUP */

/** Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 0x0;

if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}

/** Enable the WakeUp
*/
if (HAL_RTCEx_SetWakeUpTimer(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN RTC_Init 2 */

/* USER CODE END RTC_Init 2 */

}

/**
* @brief UART4 Initialization Function
* @param None
* @retval None
*/
static void MX_UART4_Init(void)
{

/* USER CODE BEGIN UART4_Init 0 */

/* USER CODE END UART4_Init 0 */

/* USER CODE BEGIN UART4_Init 1 */

/* USER CODE END UART4_Init 1 */
huart4.Instance = UART4;
huart4.Init.BaudRate = 115200;
huart4.Init.WordLength = UART_WORDLENGTH_8B;
huart4.Init.StopBits = UART_STOPBITS_1;
huart4.Init.Parity = UART_PARITY_NONE;
huart4.Init.Mode = UART_MODE_TX_RX;
huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart4.Init.OverSampling = UART_OVERSAMPLING_16;
huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart4) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN UART4_Init 2 */

/* USER CODE END UART4_Init 2 */

}

/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */

/* USER CODE END MX_GPIO_Init_1 */

/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();

/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, LED_R_Pin|LED_G_Pin, GPIO_PIN_RESET);

/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, GainSel1_Pin|GainSel2_Pin|EN_MDM_Pin|EM_Off_Pin
|pOnOff_Pin, GPIO_PIN_RESET);

/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(MCU_LED_GPIO_Port, MCU_LED_Pin, GPIO_PIN_RESET);

/*Configure GPIO pins : LED_R_Pin LED_G_Pin */
GPIO_InitStruct.Pin = LED_R_Pin|LED_G_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

/*Configure GPIO pins : GainSel1_Pin GainSel2_Pin EN_MDM_Pin EM_Off_Pin
pOnOff_Pin */
GPIO_InitStruct.Pin = GainSel1_Pin|GainSel2_Pin|EN_MDM_Pin|EM_Off_Pin
|pOnOff_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

/*Configure GPIO pins : MDM_PState_Pin MDM_IsOn_Pin */
GPIO_InitStruct.Pin = MDM_PState_Pin|MDM_IsOn_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

/*Configure GPIO pin : Temp_L_Pin */
GPIO_InitStruct.Pin = Temp_L_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(Temp_L_GPIO_Port, &GPIO_InitStruct);

/*Configure GPIO pin : V_Fu_Trig_Pin */
GPIO_InitStruct.Pin = V_Fu_Trig_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(V_Fu_Trig_GPIO_Port, &GPIO_InitStruct);

/*Configure GPIO pin : BAT_State_Pin */
GPIO_InitStruct.Pin = BAT_State_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(BAT_State_GPIO_Port, &GPIO_InitStruct);

/*Configure GPIO pin : MCU_LED_Pin */
GPIO_InitStruct.Pin = MCU_LED_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(MCU_LED_GPIO_Port, &GPIO_InitStruct);

/*Configure GPIO pins : Fu_Pos_Pin Temp_H_Pin */
GPIO_InitStruct.Pin = Fu_Pos_Pin|Temp_H_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI2_IRQn);

HAL_NVIC_SetPriority(EXTI6_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI6_IRQn);

HAL_NVIC_SetPriority(EXTI7_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI7_IRQn);

HAL_NVIC_SetPriority(EXTI12_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI12_IRQn);

HAL_NVIC_SetPriority(EXTI15_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI15_IRQn);

/* USER CODE BEGIN MX_GPIO_Init_2 */

/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void flashGreenLED(){

HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, SET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, RESET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, SET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, RESET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, SET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, RESET);
HAL_Delay(100);
}


void flashRedLED(){
HAL_GPIO_WritePin(LED_R_GPIO_Port, LED_R_Pin, SET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_R_GPIO_Port, LED_R_Pin, RESET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_R_GPIO_Port, LED_R_Pin, SET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_R_GPIO_Port, LED_R_Pin, RESET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_R_GPIO_Port, LED_R_Pin, SET);
HAL_Delay(100);
HAL_GPIO_WritePin(LED_R_GPIO_Port, LED_R_Pin, RESET);
HAL_Delay(100);

}
//__HAL_RCC_PWR_CLK_ENABLE ();
//HAL_PWREx_EnterSHUTDOWNMode();
//HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK;
//HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD);
//HAL_ADC_Start(&hadc4);
//__HAL_RCC_ADC4_CLKAM_ENABLE();
static void Enter_Stop2_Mode(void)
{

HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_SLEEPENTRY_WFI);
}



/* USER CODE END 4 */

/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
//NVIC_SystemReset();
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

MM..1
Super User
July 18, 2026

Why NVIC RESET? And primary when you suspentick after wake require resume.

Plus plac led toggle after wake to check. STOP mode is unreal test with debuger.

static void Enter_Stop2_Mode(void)
{
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_SLEEPENTRY_WFI);
...resume tick
...toggle led
}

 

yycAuthor
Associate II
August 3, 2026

Thank you for your reply!

 

I applied resume and clock config function and everything worked. However, that only applied to the code within the Enter_Stop2_Mode() function but not anything came after it. 

 

Thanks again for your suggestion.

Gyessine
ST Technical Moderator
July 20, 2026

Hello  ​@yyc 
If I understood you code correctly
Correct me if I’m wrong
I don’t see any function that re-call the system clock config or resume HAL_tick after your “enter stop mode” function
re-configuring system clock is mandatory after waking up from stop mode
can you implement something like this sequence and see what happens

static void Enter_stop2_mode(void)
{
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
SystemClock_Config();
HAL_ResumeTick();
}

BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yycAuthor
Associate II
August 3, 2026

Hello Gyessine,

 

Thank you for your suggestion. I did exactly your order. However, after one power cycle, the processor still froze after extiting the “Enter_stop2_mode()” function.

I tried putting something like the attached code, and the clock worked fine with delays within the function. Upon exiting the function everything stalled. Thank you very very much for your help.

static void Enter_stop2_mode(void)
{
MCU_IsAsleep();
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_SLEEPENTRY_WFI);
SystemClock_Config();
HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, SET);
HAL_ResumeTick();
NVIC_SystemReset();
HAL_Delay(4000);
HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, RESET);

}

 

Andrew Neil
Super User
August 3, 2026

Note that you can connect the debugger to a “frozen” system - without doing a reset or a download:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Gyessine
ST Technical Moderator
August 5, 2026

Hello ​@yyc 

This is a simple project that enters STOP2 mode when there is no activity for 3 seconds, and exits STOP2 when the blue button on PC13 is pressed.

A visual indication is provided using the blue LED on PB7:

  • PB7 ON: the system is in running mode
  • PB7 OFF: the system is in STOP mode

You can use this project as a reference for your own implementation.
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Gyessine
ST Technical Moderator
September 25, 2026

Hello ​@yyc 
Any updates
is your issue solved?
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yycAuthorBest answer
Associate II
September 25, 2026

Hello Gyessine,

 

Thank you for your followup. 

 

It turns out I need to put all of my declared variables and struct into SRAM4 by modifying the “STM32U575RITXQ_FLASH.ld” file. I noticed that the unit would get into a hard fault error state after waking up, then it turned out to be SRAM 1~3 were powered down in STOP2 mode. Only data in SRAM4 in retained by default.

 

Youyou