Skip to main content
FKaes.1
Associate III
May 12, 2025 1:09 PM UTC
Solved

STM32U5: Spi delay after start

Hello,

after setup SPI1 and setting CSTART=1, I expected that SPI is send immidiatly on bus.

(I toogled PE00 with CSTART=1)

I couldn't find some that explains that behaviour. It behave  the same, if I use DMA or writing directly to TXDR.

Do you have an idea ?

FKaes1_0-1747055255808.png

My testcode.

 SPI1->IFCR = 0xFFFF; // Clear all flags
 MODIFY_REG(SPI1->CR2, SPI_CR2_TSIZE, BufferSize);
 SPI1->CR1 |= (SPI_CR1_SPE);
 SPI1->CR1 |= SPI_CR1_CSTART;

 GPIOE->ODR &= ~(1 << 0);
 for (u32 i = 0; i < BufferSize; i++)
 {
 LL_SPI_TransmitData8(SPI1, pBuffer[i]);
 }

CPU is set to 160Mhz and SPI Prescaler is 256

 

LLECH.1
LLECH.1Best answer
ST Employee
May 14, 2025 7:19 AM UTC

Hello FKaes.1,

In fact, hardware needs 5 clock cycles to have first clock edge from CSTART assertion. It corresponds to 5*256/150 = 8µs. Therefore, the SPI behavior that you can observe is the expected one.

Best regards,

 

8 replies

ST Technical Moderator
May 12, 2025 3:09 PM UTC

Hello @FKaes.1 

This bit is set to start SPI communication. However, communication cannot start if there is no data available in the TX FIFO.

Saket_Om_0-1747062515458.png

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
FKaes.1
FKaes.1Author
Associate III
May 13, 2025 5:54 AM UTC

Hi, I changed it for testing to "front load" the FIFO with some bytes. Bu still same behavior.FKaes1_0-1747115412512.png

 SPI1->IFCR = 0xFFFF; // Clear all flags
 MODIFY_REG(SPI1->CR2, SPI_CR2_TSIZE, BufferSize);
 SPI1->CR1 |= (SPI_CR1_SPE);

 for (u32 i = 0; i < 8; i++) // front load before start
 {
 LL_SPI_TransmitData8(SPI1, pBuffer[i]);
 }

 SPI1->CR1 |= SPI_CR1_CSTART; // start

 GPIOE->ODR &= ~(1 << 0);
 for (u32 i = 8; i < BufferSize; i++) // send the remaining bytes
 {
 LL_SPI_TransmitData8(SPI1, pBuffer[i]);
 }
FKaes.1
FKaes.1Author
Associate III
May 13, 2025 12:50 PM UTC

For testing, I set the SPI Prescaler from 256 to 32. Then the delay was reduced by factor 8, too. So, I assume it is not caused by SW.

At the end, this isn't a problem for me. I was just interessed, if  this was caused by a wrong setup or usage by my side.

LLECH.1
ST Employee
May 13, 2025 1:32 PM UTC

Hello FKaes.1,

Such delay can appear if MSSI bits of CFG2 register are not set to their reset values.

Could you verify this register please ? 

Also I suppose your SPI is configured in Master mode, otherwise it is the received master clock which triggers the start of transfer and not CSTART bit.

 

Best regards,

FKaes.1
FKaes.1Author
Associate III
May 13, 2025 2:41 PM UTC

This are the settings+config rigth before setting CSTART = 1.

FKaes1_0-1747146879919.png

MSSI = 0

Master = 1

HW SS is not indented to be used. Chip select is controlled by SW.

For testing, I set MSSI to the max. value and the delay increased. So, the direction seems to be right.

 

LLECH.1
LLECH.1Best answer
ST Employee
May 14, 2025 7:19 AM UTC

Hello FKaes.1,

In fact, hardware needs 5 clock cycles to have first clock edge from CSTART assertion. It corresponds to 5*256/150 = 8µs. Therefore, the SPI behavior that you can observe is the expected one.

Best regards,

 

Visitor II
Mar 23, 2026 3:57 PM UTC

I'm using an STM32H563 microcontroller. 

I performed SPI communication with that microcontroller, and the same delay occurred. Does the H563 also experience a 5-cycle delay?

FKaes.1
FKaes.1Author
Associate III
May 14, 2025 9:08 AM UTC

ok, thank you. That explains it. I was just not able to find that in the datasheet / ref manual.