Skip to main content
Associate II
Jun 4, 2025 3:28 PM UTC
Solved

STM32N657X0 with Classic USB device middleware

I am trying to add the NUCLEO-N657X0-Q (MB194-N657X0Q-C01) to the IMBootloader project, which currently uses the Legacy Classic USB device middleware. I ran into a problem where, after calling the HAL_PCD_Start() function, I receive an unexpected interrupt.

IgorMisic_0-1749049890954.png

 

If I comment out the line

USBx_DEVICE->DCTL &= ~USB_OTG_DCTL_SDIS;

the issue no longer occurs.

Exact position of line in the code:
https://github.com/IMProject/IMBootloader/blob/add_nucleo-stm32n657x-q/Drivers/STM32N6xx_HAL_Driver/Src/stm32n6xx_ll_usb.c#L1152

The full code is available in this branch:
https://github.com/IMProject/IMBootloader/tree/add_nucleo-stm32n657x-q


It can be built with a simple command: make nucleo_n657x0_q_ram


Also attaching a video showing how the issue occurs.

Any pointers to help save time would be appreciated. Thanks in advance!

This topic has been closed for replies.

1 reply

IgorMisicAuthorBest answer
Associate II
Jun 5, 2025 5:11 PM UTC