Skip to main content
Associate III
July 3, 2025
Solved

STM32N6570-DK USB UVC Not Detected – Possible USBPD/UCPD Dependency?

Hello,

I'm working on implementing USB UVC on the STM32N6570-DK board. I generated a project using STM32CubeMX only for FSBL and added the following files manually from the ST USBX example project

1 . ux_device_video.c and .h
2 . ux_device_descriptors .c and .h
3 . app_usbx_device .c and .h
4 . app_azure_rtos.c and .h

All files were taken from this example:

https://github.com/STMicroelectronics/STM32CubeN6/tree/main/Projects/STM32N6570-DK/Applications/USBX/Ux_Device_Video/Appli 

However, I did not use USBPD/UCPD in my CubeMX configuration. The ST example uses both USBPD and UCPD and also includes a separate FSBL and Application.

Issue:

When I flash the my project to the STM32N6570-DK board, the USB device is not enumerating as a UVC device it does not appear in the Windows Device Manager at all.

I previously tested a similar setup on an STM32U5 device, and it worked — the UVC device was properly enumerated.

Questions:

  1. Is UCPD/USBPD required for USB UVC to work on the STM32N6570-DK board?

  2. Could this be the reason the USB is not being detected?

  3. Could ST provide a   .ioc   file for the UX_Device_Video example project  for reference?

Any help or clarification would be greatly appreciated!

Thank you

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
July 7, 2025

Hi @saikumar 

I assume in case, you don't use UCPD peripheral, you need to make some hardware change in schematics to pull down CC lines with 5.1KOhms and reconfigure TCPP port to type C only. Otherwise, use the second USB controller as implemented type C only. 

FBL_0-1751877719652.jpeg

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

5 replies

ST Technical Moderator
July 3, 2025

Dear @saikumar 

First, did you follow the README file and flash the provided example? Does it work as-is, or not? Without regenerating the code using CubeMX?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
saikumarAuthor
Associate III
July 4, 2025

Hello ,  mr @FBL 

Yes, I followed the README instructions and flashed the provided example without regenerating any code. It worked correctly__the UVC device was properly enumerated and appear in  Windows Device Manager, and I was able to preview the video output using the Windows Camera app.

However, when I tried to generate the project using STM32CubeMX (for FSBL only) it is not working. please check the source code and .ioc provided above .

Thank you,

ST Technical Moderator
July 4, 2025

Hi @saikumar

Currently, latest CubeMX v6.14.1 does not support USB code generation for STM32N6 in USB applications. You should refer to example provided in CubeN6 as reference.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL