Skip to main content
Associate III
Oct 7, 2026 9:47 AM UTC
Question

STM32N6570-DK + MP23DB01HP on MDF1: recommended CIC/gain/HPF/PDM-clock settings for 16 kHz audio, and start-up thump

Hi all,

I'm recording 16 kHz mono audio from the on-board digital MEMS mic (MP23DB01HP) of the STM32N6570-DK using the BSP's MDF path (MDF1, filter 0, PE2 MDF1_CCK0, PE8 MDF1_DATIN0, GPDMA1 channel 0, SPI mode, falling edge). The recording runs next to a camera/ISP pipeline, an NPU model and an H.264 encoder, so I want the audio path to cost as little CPU as possible and sound clean.

Current setup (BSP defaults for 16 kHz)

  • Kernel clock: IC8 from PLL4 = 50 MHz (HSI-based), PROCDIV = 2, CCKDIV = 12, so the PDM clock is about 2.08 MHz
  • CIC: Sinc4, R = 32; reshape filter on, ÷4 (total decimation 128)
  • Gain +2 (about +6 dB); HPF 0.000625 × fPCM (about 10 Hz)
  • Async continuous acquisition, circular DMA into a 16 KB buffer

What I tried
I built a test firmware that records one clip per MDF configuration (5 s each, one config per boot) and compared them offline. Configs: Sinc4 vs Sinc5 R = 32 (gain steps −7, −8, −9), HPF at 10, 20, 40 and 152 Hz, a PLL4 retune to 81.92 MHz with IC8 ÷ 10 for an exact 2.048 MHz PDM clock (AN5795 Table 19), and R = 16 with a 1.024 MHz PDM clock.

What I saw

  • Sinc5 at gain −8 gives the same loudness as Sinc4 at +2 (the extra CIC gain is about 30 dB, which matches the gain steps).
  • With the 10 Hz HPF, every clip has a DC offset (about 0.04 of full scale) and a start-up transient: the first 0.5 s is 10 to 12 dB louder and clips, and it decays over about 4 s. Cutoffs of 20 Hz or higher remove the DC and much of the thump.
  • R = 16 with a PDM clock of about 1 MHz gave mostly silence (about −71 dBFS) with loud bursts. The 2 MHz configs worked fine.
  • My timing is HAL-tick based, and it reports about 15.9 kHz for the 50 MHz configs and about 15.6 kHz for the retuned clock. The ratio between the two matches the design, but the absolute values are about 2.4% lower than I calculated. I think my tick is the source of the offset, but I'm not certain.

Questions

  1. Is there an official recommended MDF configuration for the MP23DB01HP at 16 kHz? Which PDM clock range and which CIC order should I use?
  2. What is the mic's start-up (power-up and ready) time? Is a thump at the start expected, and is the normal fix to discard the first few hundred milliseconds in software?
  3. Is it safe and supported to reconfigure PLL4 at runtime (as I do for the exact 2.048 MHz clock)? Is using the HSE (48 MHz) as the PLL source recommended for an accurate audio clock?
  4. Is NORMAL_SPI mode fine here, or should I use LF_MASTER_SPI as AN5795 suggests for digital mics?
  5. Any known issue with calling BSP_AUDIO_IN_DeInit followed by BSP_AUDIO_IN_Init repeatedly? In my test, the 3rd init in the same boot failed (the first two worked), so I now reboot between configs. I haven't tracked down the cause.

References: RM0486 section 35 (MDF) and Table 290, AN5795.

Thanks!

2 replies

ST Employee
Oct 13, 2026 9:20 AM UTC

Hi,
There is no official configuration, it depends on the use case targeted; near or far field, 16-bit output vs higher, etc. 
X-CUBE-AUDIO-KIT | Product - STMicroelectronics provides an example of settings for the microphone you are mentioning and the document AN5795 gives some guidances as well. 
You don’t need to for LF_MASTER_SPI unless you are targeting low power use case. This mode allows to reduce the constraint of providing the MDF with a mdf_proc_ck clock only two times higher than the sensor clock (see reference manual for more details).
Br
Jonathan 
 

Emmanuel_C
ST Employee
Oct 13, 2026 9:46 AM UTC

Hi, regarding the microphones.

First of all, be aware that MP23 microphones are Not Recommended for New Design.

According to the MP23 datasheet (find it here: MP23DB01HP | Product - STMicroelectronics), the maximum wake up time is 20 ms. On top of that there is a convergence time for the HPF filter. IT is a first order filter. This duration decreases when the cutoff frequency gets higher.

for a capture with this kind of microphone, there is no need to use a 10 Hz cutoff frequency. 40 is fine.

With 10 Hz cutoff frequency, convergence 95%= 48ms, 99% = 80 ms

With 40 Hz cutoff frequency, convergence 95%= 12ms, 99% = 20 ms

Best regards,

Emmanuel