Skip to main content
Associate II
Nov 22, 2025 1:11 PM UTC
Solved

STM32N6570-DK: HardFault when ANY peripheral is enabled with ThreadX or FreeRTOS

 

Issue Summary

On STM32N6570-DK, enabling ANY peripheral together with ThreadX or FreeRTOS causes an immediate HardFault, even in a minimal CubeMX-generated project with no user code.

This includes peripherals such as:

  • DCMIPP

  • LTDC

  • SDMMC

  • USB

  • UART

  • I2C

  • SPI

  • GPIO with interrupts

  • DMA

  • Anything beyond simple GPIO output

The issue is NOT limited to the camera/display pipeline.


Environment

  • Board: STM32N6570-DK

  • IDE: STM32CubeIDE (latest)

  • CubeMX: latest version

  • Firmware: STM32N6 HAL/BSP (latest)

  • Security Modes Tested:

    • FSBL + Application (secure/non-secure)

    • Non-secure Application only (no FSBL)

Both show the same problem.


What Works

✔ RTOS disabled → All peripherals work
✔ Camera + display pipeline works bare-metal
✔ GPIO output works with RTOS (LED blink, simple logic)


What Fails

:cross_mark:ThreadX + ANY peripheral init → HardFault
:cross_mark:FreeRTOS + ANY peripheral init → HardFault
:cross_mark:Even minimal projects with zero user code crash before scheduler start
:cross_mark:Commenting a peripheral moves the crash to the next peripheral init call

This happens even if RTOS is never started.

Example minimal code that crashes:

 

 
int main(void) 
{
HAL_Init();
SystemClock_Config(); // OK
MX_GPIO_Init(); // OK
MX_USART1_UART_Init(); // HardFault here
MX_FREERTOS_Init(); // never reached
vTaskStartScheduler(); // never reached }

Replacing UART with LTDC, DCMIPP, SDMMC, USB, SPI, etc. produces the same HardFault.


Minimal Reproduction Setup

Fresh CubeMX project → STM32N6570-DK → Non-secure application only

Enable:

  1. FreeRTOS OR ThreadX

  2. ONE peripheral (any peripheral except simple GPIO output)

Compile → Run → HardFault before entering user code.


Behavior Observed

  • HardFault occurs inside HAL init for the first peripheral that uses:

    • DMA

    • Interrupts

    • Clocks beyond basic GPIO

    • NVIC

    • Cache-sensitive memory

    • Peripheral register access

  • If DCMIPP is commented → LTDC crashes

  • If LTDC is commented → SDMMC crashes

  • If SDMMC is commented → UART crashes

This makes it clear that the RTOS + STM32N6 low-level HAL interaction is broken.


Tests Already Performed

  • Verified with both ThreadX and FreeRTOS

  • Repeated under FSBL+Application and standalone Application

  • Removed all user code

  • Removed all camera/display code

  • Moved buffers to different RAM regions

  • Disabled MPU

  • Disabled ICACHE/DCACHE

  • Disabled SysTick

  • Increased stacks and heaps

  • Checked TrustZone/NSC configuration

  • Checked RIF/Security attributes

  • Confirmed same behavior on multiple freshly created projects


Conclusion

This appears to be a system-level issue in STM32N6 RTOS integration.
CubeMX-generated startup, memory layout, low-level drivers, or TrustZone/RIF configuration may not be correctly handling RTOS environments.

The critical point is:

Any RTOS + any peripheral (beyond GPIO) = HardFault, even before scheduler start.

This is not normal, and seems like a HAL, BSP, or CubeMX integration bug specific to STM32N6.


What I Request From ST

  1. Confirm whether ThreadX and FreeRTOS are currently supported for STM32N6570 peripherals in CubeMX.

  2. Provide a working minimal example (blinky + UART) using RTOS on N6.

  3. Clarify:

    • Required MPU configuration

    • Required security / RIF / TrustZone setup

    • Required memory placement

    • Required cache settings

  4. Identify whether this is a known issue on STM32N6 with RTOS.

  5. Provide workaround or patch if available.

Saket_OmBest answer
ST Technical Moderator
Nov 24, 2025 9:07 AM UTC

Hello @JaiGanesh 

Please refer to the examples ThreadX and FreeRTOS below:

STM32CubeN6/Projects/NUCLEO-N657X0-Q/Applications/ThreadX at main · STMicroelectronics/STM32CubeN6

x-cube-freertos/Projects/NUCLEO-N657X0-Q/Applications at main · STMicroelectronics/x-cube-freertos 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

2 replies

mbarg.1
Senior III
Nov 22, 2025 3:10 PM UTC

I went in a similar problem with ThreadX.

After some debugging, I found that relates to global variables and relative initialzation not fitting correctly in assigned space.

Check sections and partitions in .ld file toward actual addresses, could be that some is overlapping and overwrite happens at start; if it is the case, change sizes to fit everything.

Some more suggestion:

check RCC register for corruption;

check stack allocation.

 

Saket_OmBest answer
ST Technical Moderator
Nov 24, 2025 9:07 AM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om