Skip to main content
Associate
June 25, 2026
Solved

STM32N657 NUCLEO standalone ROM flash boot locks, but same FSBL works via GDB launch

Summary 

 

On a NUCLEO-N657X0-Q I have a custom (non-CubeMX-template) FSBL that copies an 

"LRUN" application image from external XSPI flash into AXISRAM and jumps to it. The 

byte-identical signed FSBL runs completely when I stage it with the debugger in 

Development boot (monitor reset → load → jump Reset_Handler) — the app runs end to 

end. But in true ROM flash-boot (BOOT pins set for boot-from-flash, power-cycle, no 

debugger), the FSBL reaches main() (user LEDs light) and then locks up before its 

first clock-configuration step. The lock-up is invisible to SWD, UART, and even fault 

handlers, which points at a processor LOCKUP tied to the state the boot ROM leaves at 

the FSBL entry in flash-boot (security / RIF / clock), which differs from the debugger 

path. I would like to understand what minimal init my FSBL must do at entry in flash-boot. 

 

Hardware / tools 

 

- Board: NUCLEO-N657X0-Q (MB1940), STM32N657X0H, Cortex-M55 + Neural-ART. Device ID 0x486, Rev Z. Lifecycle state: OPEN (SWD attaches in Dev boot). 

- External flash: MX25UM51245G (XSPI2), external loader MX25UM51245G_STM32N6570-NUCLEO.stldr. 

- Tools: STM32CubeCLT 1.21.0 (arm-none-eabi-gcc 14.3.1, CMake/Ninja), STM32CubeProgrammer 2.22.0, ST-LINK gdb server. ST-LINK FW V3J17M11. 

 

Boot architecture (copy-to-RAM, single image, no XIP) 

 

Boot ROM → signed FSBL (linked + executes at 0x34180000, AXISRAM2) → configures the 

system clock → maps XSPI2 memory-mapped @50 MHz → copies the application image 

(0x70100000 → 0x34000400, AXISRAM1) → jumps to it. External-flash map: 

 

| address | image | signed | 

|---|---|---| 

| 0x70000000 | FSBL-trusted.bin (~62 KB) | yes (-hv 2.1) | 

| 0x70100000 | application (raw LRUN, ~286 KB) | no | 

| 0x70200000 | data blob (~5.8 MB) | no | 

 

The FSBL is compiled for Cortex-M55 with -mcmse (secure) but currently does no SAU / 

security-partition init (no partition_stm32n657xx.h; SystemInit does not call 

TZ_SAU_Setup). What the FSBL does after reset: HAL_Init() → light 3 user LEDs → 

HAL_RCC clock config (PLL1=800 / PLL2=600 → CPU 600 MHz, AHB 100 MHz; the ST Edge AI 

"no-overdrive" tree) → XSPI2 map → copy → jump. 

 

Signing & flashing (in Development boot, JP2 = 1) 

 

 

STM32_SigningTool_CLI -bin FSBL.bin -nk -of 0x80000000 -t fsbl -o FSBL-trusted.bin -hv 2.1 

STM32_Programmer_CLI -c port=SWD mode=UR --extload MX25UM51245G_STM32N6570-NUCLEO.stldr \ 

                     --download FSBL-trusted.bin 0x70000000 -v        # "Download verified successfully" 

 

 

What WORKS — debugger-staged launch (Development boot, JP2 = 1) 

 

Staging the identical signed FSBL and jumping to its reset vector — which reproduces the 

ROM's copy-to-RAM + jump — runs the whole chain successfully (FSBL + app, full UART output): 

 

 

ST-LINK_gdbserver -d --apid 1 -e -p 61234 -cp <CubeProgrammer\bin> 

arm-none-eabi-gdb FSBL.elf -ex "target extended-remote :61234" \ 

   -ex "monitor reset" -ex "load" -ex "jump Reset_Handler" 

 

 

What FAILS — true ROM flash-boot (no debugger) 

 

Set the BOOT pins for boot-from-flash (on this board JP1 = 0, JP2 = 0), full power-cycle, 

no debugger. Result: the FSBL runs (the 3 user LEDs light at main()), then locks up 

before the first clock-config step (an LED probe that would turn off at clock-config entry 

never executes). Evidence that it is a LOCKUP, not a recoverable hang or fault: 

 

- SWD will not attach in flash-boot: STM32_Programmer_CLI -c port=SWD mode=HotPlug → "No STM32 target found." 

- UART is silent: both HAL UART and a bare-metal, HSI-clocked, polled USART1 (PE5/PE6, no HAL/SysTick/IRQ) placed *immediately after* the (confirmed-reached) LED init emit nothing. 

- Fault handlers never fire: I installed LED-encoded HardFault/MemManage/BusFault/UsageFault/SecureFault handlers (with SCB->SHCSR MEM/BUS/USG/SECUREFAULTENA set) whose first action turns all LEDs off and then blinks a code. They never run — the LEDs main() set stay frozen. A fault that never reaches its handler ⇒ processor lockup. 

- 5-minute wait: no progress, no output. 

 

What I have already ruled out 

 

- Forcing HSI on first; an HSI-park preamble; several clock trees. 

- ST-style MPU_config (mark 0x70000000 Normal/RO/exec, enable MPU). 

- HAL_PWREx_ConfigSupply(PWR_EXTERNAL_SOURCE_SUPPLY) (confirmed correct supply mode for this board — external TPS62864) and __enable_irq(). 

- The boot provisioning is working: the ROM loads + launches the signed FSBL (main runs), so this is not a boot-address/signature problem. Option bytes are N/A (-ob displ → *"not supported for STM32N6"*; the N6 uses BSEC OTP / lifecycle). 

- The same image runs fully via the gdb-staged jump Reset_Handler, so it is not the FSBL or application *logic* — it is the entry-state the ROM leaves in flash-boot. 

 

Questions 

 

1. In a true ROM flash-boot, what security / RIF / RISAF / clock state does the boot ROM leave at the FSBL entry that differs from the Development-boot jump Reset_Handler path, and that could cause a secure-context lockup when the FSBL accesses peripherals (USART1 / RCC) or reconfigures clocks? 

2. Is there a required minimal secure init (SAU partition, RIFSC, RISAF, IAC) that an FSBL must perform at entry in flash-boot but that the debugger-staged path does not require? 

3. Is a custom copy-to-RAM FSBL supported for ROM flash-boot, or must the FSBL follow ST's reference SNS secure-boot structure (secure FSBL → secure app → non-secure)? 

4. Is there a documented difference in the ROM → FSBL handoff entry-state between Dev boot (debugger) and flash boot that explains *"byte-identical image runs via gdb-staged jump Reset_Handler but locks up via ROM flash-boot"*? 

 

Any pointer to the N6 boot-from-flash FSBL requirements (beyond signing + placement at 

0x70000000) would be greatly appreciated.

RomainR.
RomainR.Best answer
ST Employee
June 25, 2026

Hello ​@Jibril 

You are using a custom FSBL. It works correctly in debug mode because it is loaded directly into AXISRAM2 by the debugger, without going through the BootROM and the external serial flash.

However, if it does not execute correctly, or does not execute at all when booting from flash via the BootROM, are you sure that the FSBL is actually being executed?
Can you debug it in flash boot mode, does the custom FSBL configure correctly the XSPI2 on XSPIM-P2 for the external flash?
Check this article:

Based on the information provided during the signing of your binaries, I believe you are not using the correct commands to sign them. The header version should be -v 2.3 instead of 2.1. In addition, with STM32CubeProgrammer v2.22.0, the --align option must be used.

Please refer to the following announcement:

If there is any doubt that the issue may be related to your FSBL, could you compile, sign (as explained above), and flash the FSBL provided here:

https://github.com/STMicroelectronics/STM32CubeN6/tree/main/Projects/NUCLEO-N657X0-Q/Templates/Template_FSBL_LRUN
 

You can also refer to this article:

Best regards,

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

RomainR.
RomainR.Best answer
ST Employee
June 25, 2026

Hello ​@Jibril 

You are using a custom FSBL. It works correctly in debug mode because it is loaded directly into AXISRAM2 by the debugger, without going through the BootROM and the external serial flash.

However, if it does not execute correctly, or does not execute at all when booting from flash via the BootROM, are you sure that the FSBL is actually being executed?
Can you debug it in flash boot mode, does the custom FSBL configure correctly the XSPI2 on XSPIM-P2 for the external flash?
Check this article:

Based on the information provided during the signing of your binaries, I believe you are not using the correct commands to sign them. The header version should be -v 2.3 instead of 2.1. In addition, with STM32CubeProgrammer v2.22.0, the --align option must be used.

Please refer to the following announcement:

If there is any doubt that the issue may be related to your FSBL, could you compile, sign (as explained above), and flash the FSBL provided here:

https://github.com/STMicroelectronics/STM32CubeN6/tree/main/Projects/NUCLEO-N657X0-Q/Templates/Template_FSBL_LRUN
 

You can also refer to this article:

Best regards,

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JibrilAuthor
Associate
July 2, 2026

Hi Romain,

Confirmed — that was exactly the issue.

Signing with -hv 2.3 and --align using STM32CubeProgrammer v2.22.0 fixed the standalone boot. The FSBL now runs the full chain from a cold, debugger-less power-up, matching the debugger-staged behavior.

For context, we had isolated the failure to the boot ROM → FSBL handoff. Reset_Handler was not executing during ROM flash boot. Your note about the header version pointed us to the real cause: the v2.1 header we reused from another board example was being silently rejected by the boot ROM.

Switching to v2.3 with --align resolved it completely. We verified the full application chain, including both models, running standalone.

Really appreciate the quick turnaround. It saved us from going down a much longer secure-boot path based on the wrong diagnosis.

Thanks,
Jibril