Skip to main content
Senior
Jul 15, 2025 11:26 AM UTC
Question

STM32N6 VENC_JPEG_Encoding issues

Hi everyone, 
I am trying to run VENC_JPEG_Encoding project using STM32CubeIDE on STM32N6570-DK board, but it is not saving .bmp as stated in README file. Upon further debugging I can see in main.c in function save_file() that it is only supported on IAR system. 

int8_t save_file(char *pName,uint8_t *pStream,uint32_t szOut)
{
 int8_t ret = 0;
#if defined ( __ICCARM__ )
 /* stdio FILE works only on IAR system */
 FILE *pFile;
 pFile = fopen(pName,"wb");
 if(pFile)
 {
 while(szOut)
 {
 uint32_t blk = 1024;
 if(szOut < blk ) blk = szOut; 
 uint32_t written = fwrite(pStream,1,blk,pFile);
 szOut-= written;
 pStream+=written;
 } 
 fclose(pFile);
 ret = 1;
 printf("the file %s is in the current folder",pName); 
 }
#endif
 return ret;
}


so how do i test it in CubeIDE as I am on Ubuntu and IAR doesnt supports Ubuntu till now.
Kindly help

3 replies

ST Technical Moderator
Jul 15, 2025 2:43 PM UTC

Hello @athern27 

I reported this internally and will get back to you as soon as possible.

Internal ticket number: 214131 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
athern27Author
Senior
Nov 21, 2025 5:24 AM UTC

@Saket_Om Any updates??

ST Technical Moderator
Nov 21, 2025 8:16 AM UTC

Hello @athern27 

Unfortunately, the issue still under investigation internally. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om